IMX8MP Android 11 Bluetooth AW-CM276NF

cancel
Showing results for 
Search instead for 
Did you mean: 

IMX8MP Android 11 Bluetooth AW-CM276NF

744 Views
VeeraH
Contributor I

Hi,

We are trying to bring up bluetooth on IMX8MP board  over UART1.

Added into Kernel command line:

BOARD_KERNEL_CMDLINE += androidboot.bt_uart=/dev/ttymxc0 androidboot.btmacaddr=2f:0b:a1:aa:bf:04

Added UART into device tree.

When we try to enable the bluetooth on Android UI, we are getting the following crash on logcat,

07-20 09:04:13.504 2066 2093 E bt_btif_config: Config is missing adapter section
07-20 09:04:13.504 2066 2093 E droid.bluetoot: [0720/090413.504592:ERROR:config.cc(104)] config_new: unable to open file '/data/misc/bluedroid/bt_config.bak': No such file or directory
07-20 09:04:13.504 2066 2093 E bt_btif_config_transcode: btif_config_transcode unable to load XML file '/data/misc/bluedroid/bt_config.xml': 3
07-20 09:04:13.504 2066 2093 E bt_btif_config: init unable to transcode legacy file; creating empty config.
07-20 09:04:13.511 2066 2098 E bt_btif_storage: btif_storage_get_adapter_property: Controller not ready! Unable to return Bluetooth Address
07-20 09:04:13.511 2066 2098 E BluetoothServiceJni: adapter_properties_callback: Status 1 is incorrect
07-20 09:04:16.555 2066 2096 E bt_hci : startup_timer_expired
--------- beginning of crash
07-20 09:04:16.556 391 418 F libc : Fatal signal 6 (SIGABRT), code -1 (SI_QUEUE) in tid 418 (HwBinder:391_2), pid 391 (bluetooth@1.0-s)
07-20 09:04:16.608 2116 2116 F DEBUG : *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
07-20 09:04:16.609 2116 2116 F DEBUG : Build fingerprint: 'Android/evk_8mp/evk_8mp:11/RQ1A.201205.003/eng.adlink.20220708.175229:userdebug/dev-keys'
07-20 09:04:16.609 2116 2116 F DEBUG : Revision: '0'
07-20 09:04:16.609 2116 2116 F DEBUG : ABI: 'arm64'
07-20 09:04:16.610 2116 2116 F DEBUG : Timestamp: 2022-07-20 09:04:16+0000
07-20 09:04:16.610 2116 2116 F DEBUG : pid: 391, tid: 418, name: HwBinder:391_2 >>> /vendor/bin/hw/android.hardware.bluetooth@1.0-service <<<
07-20 09:04:16.610 2116 2116 F DEBUG : uid: 1002
07-20 09:04:16.610 2116 2116 F DEBUG : signal 6 (SIGABRT), code -1 (SI_QUEUE), fault addr --------
07-20 09:04:16.610 2116 2116 F DEBUG : x0 0000000000000000 x1 00000000000001a2 x2 0000000000000006 x3 0000ffcbe7758520
07-20 09:04:16.610 2116 2116 F DEBUG : x4 fefeff282764726e x5 fefeff282764726e x6 fefeff282764726e x7 7f7f7f7f7f7f7f7f
07-20 09:04:16.610 211[ 2182.018593] init: Untracked pid 2116 exited with status 0
6 2116 F DEBUG : x8 00000[ 2182.026796] binder: release 391:391 transaction 105596 in, still active
000000000f0 x9 0000ffcdf8d3b800[ 2182.026946] init: Service 'vendor.bluetooth-1-0' (pid 391) received signal 6
x10 ffffff80ffffffdf x11 00000[ 2182.036107] binder: send failed reply for transaction 105596 to 2066:2111
00000000001
07-20 09:04:16.610 [ 2182.046212] init: Sending signal 9 to service 'vendor.bluetooth-1-0' (pid 391) process group...
2116 2116 F DEBUG : x12 00[ 2182.068388] libprocessgroup: Successfully killed process cgroup uid 1002 pid 391 in 0ms
00ffcbe7758010 x13 0000000000000[ 2182.071067] binder: release 391:418 transaction 107716 in, still active
016 x14 0000ffcbe7758198 x15 00[ 2182.079000] init: Untracked pid 2118 exited with status 0
0000007d000000
07-20 09:04:16.61[ 2182.087465] binder: send failed reply for transaction 107716 to 2066:2096
0 2116 2116 F DEBUG : x16[ 2182.099349] init: starting service 'vendor.bluetooth-1-0'...
0000ffcdf8dd4c80 x17 0000ffcdf8db63c0 x18 0000ffcbe73fc000 x19 00000000000000ac
07-20 09:04:16.610 2116 2116 F DEBUG : x20 0000000000000187 x21 00000000000000b2 x22 00000000000001a2 x23 00000000ffffffff
07-20 09:04:16.611 2116 2116 F DEBUG : x24 0000ffcbe7759000 x25 0000ffcbe7758998 x26 0000ffcbe7759000 x27 0000000000000000
07-20 09:04:16.611 2116 2116 F DEBUG : x28 00000000000fc000 x29 0000ffcbe77585a0
07-20 09:04:16.611 2116 2116 F DEBUG : lr 0000ffcdf8d69544 sp 0000ffcbe7758500 pc 0000ffcdf8d69574 pst 0000000000000000
07-20 09:04:16.633 2116 2116 F DEBUG : backtrace:
07-20 09:04:16.633 2116 2116 F DEBUG : #00 pc 000000000004e574 /apex/com.android.runtime/lib64/bionic/libc.so (abort+180) (BuildId: f81965d884d6ebc5e5c3fd825c17a209)
07-20 09:04:16.633 2116 2116 F DEBUG : #01 pc 00000000000079f0 /vendor/lib64/hw/android.hardware.bluetooth@1.0-impl.so (std::__1::__throw_bad_function_call()+8) (BuildId: e0b742ea3831890d06f5)
07-20 09:04:16.633 2116 2116 F DEBUG : #02 pc 0000000000006900 /vendor/lib64/hw/android.hardware.bluetooth@1.0-impl.so (android::hardware::bluetooth::V1_0::implementation::BluetoothHci::close)
07-20 09:04:16.633 2116 2116 F DEBUG : #03 pc 0000000000013558 /apex/com.android.vndk.v30/lib64/android.hardware.bluetooth@1.0.so (android::hardware::bluetooth::V1_0::BnHwBluetoothHci::_hidl_)
07-20 09:04:16.633 2116 2116 F DEBUG : #04 pc 0000000000013964 /apex/com.android.vndk.v30/lib64/android.hardware.bluetooth@1.0.so (android::hardware::bluetooth::V1_0::BnHwBluetoothHci::onTran)
07-20 09:04:16.633 2116 2116 F DEBUG : #05 pc 0000000000094ae8 /apex/com.android.vndk.v30/lib64/libhidlbase.so (android::hardware::BHwBinder::transact(unsigned int, android::hardware::Parcel )
07-20 09:04:16.633 2116 2116 F DEBUG : #06 pc 0000000000098b9c /apex/com.android.vndk.v30/lib64/libhidlbase.so (android::hardware::IPCThreadState::getAndExecuteCommand()+1076) (BuildId: a108a)
07-20 09:04:16.633 2116 2116 F DEBUG : #07 pc 0000000000099df8 /apex/com.android.vndk.v30/lib64/libhidlbase.so (android::hardware::IPCThreadState::joinThreadPool(bool)+96) (BuildId: a108af492)
07-20 09:04:16.633 2116 2116 F DEBUG : #08 pc 00000000000a8ff0 /apex/com.android.vndk.v30/lib64/libhidlbase.so (android::hardware::PoolThread::threadLoop()+24) (BuildId: a108af492dfd57b616484)
07-20 09:04:16.633 2116 2116 F DEBUG : #09 pc 000000000001567c /apex/com.android.vndk.v30/lib64/libutils.so (android::Thread::_threadLoop(void*)+260) (BuildId: d1997a8c7b581c47382e2b8064338bf)
07-20 09:04:16.634 2116 2116 F DEBUG : #10 pc 0000000000014f14 /apex/com.android.vndk.v30/lib64/libutils.so (thread_data_t::trampoline(thread_data_t const*)+412) (BuildId: d1997a8c7b581c47382)
07-20 09:04:16.634 2116 2116 F DEBUG : #11 pc 00000000000b0c08 /apex/com.android.runtime/lib64/bionic/libc.so (__pthread_start(void*)+64) (BuildId: f81965d884d6ebc5e5c3fd825c17a209)
07-20 09:04:16.634 2116 2116 F DEBUG : #12 pc 00000000000505d0 /apex/com.android.runtime/lib64/bionic/libc.so (__start_thread+64) (BuildId: f81965d884d6ebc5e5c3fd825c17a209)
07-20 09:04:16.697 374 374 E tombstoned: Tombstone written to: /data/tombstones/tombstone_00
07-20 09:04:16.738 2066 2111 F HidlStatus: Status.cpp:143] Failed HIDL return status not checked. Usually this happens because of a transport error (error parceling, binder driver, or from unparceling'
07-20 09:04:16.738 2066 2111 F libc : Fatal signal 6 (SIGABRT), code -1 (SI_QUEUE) in tid 2111 (bt_hci_thread), pid 2066 (droid.bluetooth)
07-20 09:04:16.788 2066 2096 E bt_hci : hci_close: Error closing the Bluetooth HAL
07-20 09:04:16.836 2125 2125 F DEBUG : *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
07-20 09:04:16.836 2125 2125 F DEBUG : Build fingerprint: 'Android/evk_8mp/evk_8mp:11/RQ1A.201205.003/eng.adlink.20220708.175229:userdebug/dev-keys'
07-20 09:04:16.837 2125 2125 F DEBUG : Revision: '0'
07-20 09:04:16.837 2125 2125 F DEBUG : ABI: 'arm64'
07-20 09:04:16.837 2125 2125 F DEBUG : Timestamp: 2022-07-20 09:04:16+0000
07-20 09:04:16.837 2125 2125 F DEBUG : pid: 2066, tid: 2111, name: bt_hci_thread >>> com.android.bluetooth <<<
07-20 09:04:16.837 2125 2125 F DEBUG : uid: 1002
07-20 09:04:16.837 2125 2125 F DEBUG : signal 6 (SIGABRT), code -1 (SI_QUEUE), fault addr --------
07-20 09:04:16.838 2125 2125 F DEBUG : Abort message: 'Failed HIDL return status not checked. Usually this happens because of a transport error (error parceling, binder driver, or from unparceling).'
07-20 09:04:16.838 2125 2125 F DEBUG : x0 0000000000000000 x1 000000000000083f x2 0000000000000006 x3 0000e1bfc28f52b0
07-20 09:04:16.838 2125 2125 F DEBUG : x4 0000000000000000 x5 0000000000000000 x6 0000000000000000 x7 7f7f7f7f7f7f7f7f
07-20 09:04:16.838 2125 2125 F DEBUG : x8 00000000000000f0 x9 0000e1c24dc21800 x10 ffffff80fffffbdf x11 0000000000000001
07-20 09:04:16.838 2125 2125 F DEBUG : x12 0000e1bfc28f4160 x13 00000000000001a6 x14 0000e1bfc28f4210 x15 000000007d000000
07-20 09:04:16.838 2125 2125 F DEBUG : x16 0000e1c24dcbac80 x17 0000e1c24dc9c3c0 x18 0000e1bfc263a020 x19 00000000000000ac
07-20 09:04:16.838 2125 2125 F DEBUG : x20 0000000000000812 x21 00000000000000b2 x22 000000000000083f x23 00000000ffffffff
07-20 09:04:16.838 2125 2125 F DEBUG : x24 00000000746c7561 x25 0000e1bfc28f6000 x26 b400e1c0fc258848 x27 0000e1bfd31747b8
07-20 09:04:16.838 2125 2125 F DEBUG : x28 0000e1c03c1b7000 x29 0000e1bfc28f5330
07-20 09:04:16.838 2125 2125 F DEBUG : lr 0000e1c24dc4f544 sp 0000e1bfc28f5290 pc 0000e1c24dc4f574 pst 0000000000000000
07-20 09:04:16.924 2125 2125 F DEBUG : backtrace:
07-20 09:04:16.925 2125 2125 F DEBUG : #00 pc 000000000004e574 /apex/com.android.runtime/lib64/bionic/libc.so (abort+180) (BuildId: f81965d884d6ebc5e5c3fd825c17a209)
07-20 09:04:16.925 2125 2125 F DEBUG : #01 pc 00000000005647e8 /apex/com.android.art/lib64/libart.so (art::Runtime::Abort(char const*)+2320) (BuildId: 07e9d1b6c845ed0756a71370c009243a)
07-20 09:04:16.925 2125 2125 F DEBUG : #02 pc 0000000000013ab0 /system/lib64/libbase.so (android::base::SetAborter(std::__1::function<void (char const*)>&&)::$_3::__invoke(char const*)+80) (B)
07-20 09:04:16.925 2125 2125 F DEBUG : #03 pc 0000000000013090 /system/lib64/libbase.so (android::base::LogMessage::~LogMessage()+320) (BuildId: 6d398535cd6d9315930f056432520bb9)
07-20 09:04:16.925 2125 2125 F DEBUG : #04 pc 000000000005440c /system/lib64/libhidlbase.so (android::hardware::details::return_status::assertOk() const+236) (BuildId: 525e3e8749b695911bbea61)
07-20 09:04:16.925 2125 2125 F DEBUG : #05 pc 0000000000054450 /system/lib64/libhidlbase.so (android::hardware::details::return_status::~return_status()+48) (BuildId: 525e3e8749b695911bbea612)
07-20 09:04:16.925 2125 2125 F DEBUG : #06 pc 00000000002665f0 /system/lib64/libbluetooth.so (hci_initialize()+864) (BuildId: 1386fc50507bfea1c9b40e68d9f361ca)
07-20 09:04:16.925 2125 2125 F DEBUG : #07 pc 000000000009e8a0 /system/lib64/libchrome.so (base::debug::TaskAnnotator::RunTask(char const*, base::PendingTask*)+192) (BuildId: c0d8f6d7d8e62550)
07-20 09:04:16.925 2125 2125 F DEBUG : #08 pc 00000000000bf024 /system/lib64/libchrome.so (base::MessageLoop::RunTask(base::PendingTask*)+324) (BuildId: c0d8f6d7d8e625506d14a3ec12a127cc)
07-20 09:04:16.925 2125 2125 F DEBUG : #09 pc 00000000000bf3d0 /system/lib64/libchrome.so (base::MessageLoop::DoWork()+464) (BuildId: c0d8f6d7d8e625506d14a3ec12a127cc)
07-20 09:04:16.925 2125 2125 F DEBUG : #10 pc 00000000000c0bd0 /system/lib64/libchrome.so (base::MessagePumpDefault::Run(base::MessagePump::Delegate*)+104) (BuildId: c0d8f6d7d8e625506d14a3ec1)
07-20 09:04:16.926 2125 2125 F DEBUG : #11 pc 00000000000e3274 /system/lib64/libchrome.so (base::RunLoop::Run()+84) (BuildId: c0d8f6d7d8e625506d14a3ec12a127cc)
07-20 09:04:16.926 2125 2125 F DEBUG : #12 pc 00000000001a3494 /system/lib64/libbluetooth.so (bluetooth::common::MessageLoopThread::Run(std::__1::promise<void>)+268) (BuildId: 1386fc50507bfea)
07-20 09:04:16.926 2125 2125 F DEBUG : #13 pc 00000000001a2fd8 /system/lib64/libbluetooth.so (bluetooth::common::MessageLoopThread::RunThread(bluetooth::common::MessageLoopThread*, std::__1::)
07-20 09:04:16.926 2125 2125 F DEBUG : #14 pc 00000000001a399c /system/lib64/libbluetooth.so (void* std::__1::__thread_proxy<std::__1::tuple<std::__1::unique_ptr<std::__1::__thread_struct, st)
07-20 09:04:16.926 2125 2125 F DEBUG : #15 pc 00000000000b0c08 /apex/com.android.runtime/lib64/bionic/libc.so (__pthread_start(void*)+64) (BuildId: f81965d884d6ebc5e5c3fd825c17a209)
07-20 09:04:16.926 2125 2125 F DEBUG : #16 pc 00000000000505d0 /apex/com.android.runtime/lib64/bionic/libc.so (__start_thread+64) (BuildId: f81965d884d6ebc5e5c3fd825c17a209)
07-20 09:04:17.614 2066 2090 E AdapterState: BLE_TURNING_ON : BLE_START_TIMEOUT
07-20 09:04:18.372 374 374 E tombstoned: Tombstone written to: /data/tombstones/tombstone_01
[ 2183.736418] init: Untracked pid 2125 exited with status 0
[ 2183.750869] init: Untracked pid 2128 exited with status 0
07-20 09:04:18.456 565 601 E BluetoothManagerService: MESSAGE_BLUETOOTH_SERVICE_DISCONNECTED(1)

 

Please share your inputs.

Thanks,

Hariharan.V.

0 Kudos
7 Replies

636 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi @VeeraH ,

 

1. Don't add any other buledroid stack to NXP Android BSP.

2. For andrdoid 11, Bluedroid stack is in system/bt 

weidong_sun_0-1661218137356.png

3. Even if NXP android 11 also supports SD8997 , default firmware is not suitable for you application.

~/android_11.0.0_2.6.0/vendor/nxp-opensource/nxp-mwifiex/mxm_wifiex/wlan_src/Makefile

# Multi-chipsets
CONFIG_SD8887=n
CONFIG_SD8897=n
CONFIG_USB8897=n
CONFIG_PCIE8897=n
CONFIG_SD8977=n
CONFIG_SD8978=y
CONFIG_USB8978=n
CONFIG_SD8997=y
CONFIG_USB8997=n
CONFIG_PCIE8997=y
CONFIG_SD8987=y
CONFIG_SD9097=n
CONFIG_SD9177=n
CONFIG_SD8801=y
CONFIG_USB8801=n
CONFIG_USB9097=n
CONFIG_PCIE9097=n
CONFIG_SD9098=n
CONFIG_USB9098=n
CONFIG_PCIE9098=y

BUT default firmware "~/android_11.0.0_2.6.0/vendor/nxp/imx-firmware/nxp/FwImage_8997/pcieuart8997_combo_v4.bin", only supports PCIe For wifi & UART For BT

4. Would you please tell me your current driver version? (full version, please!)

5. Since you have NDA with NXP, create a new case in SFDC, let us discuss it in the system.

 

Regards,

weidong

 

 

0 Kudos

725 Views
VeeraH
Contributor I

Hi,

We have some hardware issue with accessing bluetooth over serial port.

Please share your inputs whether it is possible to use SDSD access of wifi over SDIO and bluetooth over SDIO on android 11.

 

0 Kudos

720 Views
VeeraH
Contributor I

Bluetooth driver is up using SDIO interface as below,

 

evk_8mp:/ # hciconfig
hci0: Type: SDIO
BD Address: 00:E9:3A:9B:09:18 ACL MTU: 1021:7 SCO MTU: 120:6
UP RUNNING
RX bytes:1356 acl:0 sco:0 events:82 errors:0
TX bytes:1205 acl:0 sco:0 commands:82 errors:0

 

But when we try to enable / on bluetooth via android UI, it does not working.

please share your inputs.

0 Kudos

668 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @VeeraH ,

 

If you want to use SDIO interface for Bluetooth. Driver will register it as a char device. Like below.

/dev/mbtchar0 

it's usage is similar to that of UART.

 

Regards,

weidong

0 Kudos

665 Views
VeeraH
Contributor I

Hi,

We are loading the following modules in sequence,

1. mlan.ko

2. bt8xxx.ko

3. moal.ko

We are getting following instance wlan0, wlan1, p2p0, hci0 only and no /dev/mbtchar0 got created.

Please share your inputs whether we have to load any other module to get /dev/mbtchar0 and please help to get the latest device driver.

Thanks,

Veera.H.

0 Kudos

655 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi @VeeraH ,

These 2 files is WIFI driver.

1. mlan.ko

2. moal.ko

This is Bluetooth driver

1. bt8xxx.ko

In default android 11 bsp, Bluetooth uses android default one. in kernel , it is bt_uart.ko , probably, you should remove it in linux kernel configuration.

you can try the following steps:

1. Loading bt8xxx.ko driver with bt firmware.

if it is successful, check if mbtchar0 is created in /dev/ path.

2. Loading wifi driver with wifi firmare 

[Note]

(1)don't use combo firmware.

(2) you had better correct hareware issue of UART, and continue to use UART interface. because 8MP+android 11 supports 88W8997 PCIE UART by default.

[In additon]

If you have NDA and obtained NXP authorization, you can download the driver or other materials you need from our website.

 

Regards,

weidong

 

0 Kudos

640 Views
VeeraH
Contributor I

Hi,

We have NDA with NXP, and we could not find the Bluetooth bluedroid based driver in NXP portal.

Please help us to get the latest driver from the portal.

We tried to use this bluedroid driver => https://github.com/hardkernel/buildroot_vendor_marvell_bt_sd8977/tree/aml64_buildroot_master/bluedro...

we ported for the 5.10.72 kernel and getting crash after the bluetooth firmware is downloaded.

Please share your inputs.

Thanks

Veera.H.

0 Kudos