IMX8MM-evk Android11 - Reset GIPO pin for TLV320AIC3100 audio codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM-evk Android11 - Reset GIPO pin for TLV320AIC3100 audio codec

804 Views
divyeshmarne0
Contributor III

Hi Team,

Need your help to find out RESET-GIPO for TLV320AIC3100 audio codec.

I have made following changes in DTSI file:

tlv320aic31xx: codec@18 {
compatible = "ti,tlv320aic310x","ti,tlv320aic3100";
reg = <0x18>;
#sound-dai-cells = <0>;
/* Regulators */
HPVDD-supply = <&reg_3p3v>;
SPRVDD-supply = <&reg_3p3v>;
SPLVDD-supply = <&reg_3p3v>;
AVDD-supply = <&reg_3p3v>;
IOVDD-supply = <&reg_3p3v>;
DVDD-supply = <&reg_1p8v>;
};

 

LOGS:

Line 453: 10-18 09:43:02.729 0 0 D : Divyesh -tlv320aic31xx Enter Func:aic31xx_reset gpio_reset: 0
Line 454: 10-18 09:43:02.731 0 0 E tlv320aic31xx-codec 1-0018: Could not reset device: -6
Line 455: 10-18 09:43:02.737 0 0 E tlv320aic31xx-codec 1-0018: Unable to sync registers 0x9f-0x9f. -6
Line 456: 10-18 09:43:02.745 0 0 E tlv320aic31xx-codec 1-0018: Failed to restore cache: -6

 

Could pls suggest any solution for it?

Thanks

0 Kudos
2 Replies

794 Views
igorpadykov
NXP Employee
NXP Employee

Hi Divyesh

 

one can look at TLV320 example on

https://community.nxp.com/t5/i-MX-Processors/SAI-on-i-MX8M-Mini/m-p/959805

 

Best regards
igor

0 Kudos

773 Views
divyeshmarne0
Contributor III

Hi have given proper gpio reset pin number. still same error we are getting.

E tlv320aic31xx-codec 1-0018: Unable to sync registers 0x9f-0x9f. -6
E tlv320aic31xx-codec 1-0018: Failed to restore cache: -6

0 Kudos