Hello.
I have a custom imx8mm board with a 512MB DDR4 (K4A4G165WE-BCTD).
I want to do the DDR stress test (following the User guide). For that, I configured the DDR4 parameters in the MX8M_Mini_DDR4_RPA_v20.xls
I did the calibration with these parameters in the Mscale DDR Tool:
But whhen I tried to do the Stress Test, it stuck's here:
Downloading file 'bin\ddr4_train1d_string_v201709.bin' ..Done
Downloading file 'bin\ddr4_train2d_string_v201709.bin' ..Done
Downloading file 'bin\ddr4_imem_1d_v201709.bin' ..Done
Downloading file 'bin\ddr4_dmem_1d_v201709.bin' ..Done
Downloading file 'bin\ddr4_imem_2d_v201709.bin' ..Done
Downloading file 'bin\ddr4_dmem_2d_v201709.bin' ..Done
Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done
Download is complete
Waiting for the target board boot...
===================hardware_init=====================
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:30:14
*************************************************************************
Waiting for board configuration from PC-end...
--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug
- VMCR Check:
- ttbr0_el3: 0x93d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122
- MMU and cache setup complete
*************************************************************************
ARM clock(CA53) rate: 1200MHz
DDR Clock: 1200MHz
============================================
DDR configuration
DDR type is DDR4
Data width: 16, bank num: 8
For DDR4, bank num is the total of 2 bank groups and 4 banks per group
Row size: 15, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 512MB
Density per controller is: 512MB
Total density detected on the board is: 512MB
============================================
MX8M-mini: Cortex-A53 is found
*************************************************************************
============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1200Mhz...
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @533Mhz...
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 2D-Training @1200Mhz...
[Process] End of initialization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Result] PASS
============ Step 2: DDR memory accessing... ============
Verifying DDR frequency point0@1200MHz.......Pass
Verifying DDR frequency point1@533MHz.......Pass
[Result] OK
============ Step 3: DDR parameters processing... ============
[Result] Done
Success: DDR Calibration completed!!!
DDR Stress Test Iteration 1
--------------------------------
--Running DDR test on region 1--
--------------------------------
t0.1: data is addr test
Can you help me? What I'm doing wrong?
Thanks.
Could you share us the DDR datasheet to us?
Of course.
https://download.semiconductor.samsung.com/resources/data-sheet/DS_K4A4G165WE_BC_I_Rev1_4-1.pdf
All the documentation are is here:
https://semiconductor.samsung.com/us/dram/ddr/ddr4/k4a4g165we-bctd/
Thanks.
Your configuration is right, how about your status in your side?
I will help check.