IMX6ULL裸机开发程序烧写问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL裸机开发程序烧写问题

1,354件の閲覧回数
liqi_wu
Contributor III

我目前使用IMX6ULL开发板进行裸机开发,首先我使用JTAG在线调试下载,能把代码烧写到RAM中调试。我使用JTAG把代码下载到QSPI FLASH中时无法启动。后来我参考《Getting Started with MCUXpresso
SDK for i.MX 6ULL Derivatives》使用MFGTool烧写代码,结果烧写不进去,看log提示一直在reset。

//MFG 界面

pastedImage_2.png

//串口打印log

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:37:48 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:37:48 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 46C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:37:48 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 46C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:37:48 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Sep 16 2016 - 18:37:48 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC:

我刚开始玩IMX6ULL裸机开发,请各位大神多多帮忙!

ラベル(2)
0 件の賞賛
1 返信

978件の閲覧回数
liqi_wu
Contributor III

问题解决了,是由于我的JLINK还连在JTAG上面,虽然JLNIK没有连接电脑,但是干扰了USB OTG下载,导致MFG Tool无法下载image到开发板。把JLINK拔掉就可以使用MFG Tool下载image了。

0 件の賞賛