Hi everyone:
I want to two LVDS display , LVDS1 is 1080P60 output ,and LVDS2 is no HD output ,such as 1024*768, does the IMX6DL support? thanks very much 。
Hi igorpadykov
Thanks very much for your reply。so it can support one hdmi output and one lvds output at the same time ? such as 1080P60 HDMI output and 1366*768 LVDS output, thanks very much。
yes it is supported, more details can be found in presentation
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
Hi song
I am afraid not, please check performance characteristics on
sect.40.4.1 Input Parallel Display Ports i.MX6SDL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
"For dual input data interface case: Up to 85 MHz per interface. (WXGA 1366x768 @
60 frames per second, 35% blanking)."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------