IMX6 ULL系列能否实现OSD功能,SDK中有实现OSD功能的库吗?
Hi,
The i.MX6ULL support Electrophoretic display controller support direct-driver for E-Ink EPD panel, and the follows
But the i.MX6ULL processor does not have the graphics acceleration in hardware, so no OSD work.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
i.MX 6UltraLite Applications Processor Reference Manual文档如下章节,应当是可以实现简单的OSD的:
9.1.1 PiXel Processing Pipeline
The pixel processing pipeline is used to perform image processing on image/video
buffers before sending to an LCD display.
The main features of PXP include: