I can't set the 6K or 10K bitrate using the imx6ull.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't set the 6K or 10K bitrate using the imx6ull.

890 Views
zcx891106
Contributor I

I am using the imx6ull .I want to set the low CAN bitrate ,such as 6K or 10K. But I can't set it. If I set the bitrate which above the 20K, it is right. 

0 Kudos
2 Replies

803 Views
igorpadykov
NXP Employee
NXP Employee

Hi cx

one can try to select suitable reference clock:

Socket-CAN Users - selecting the clock source for FlexCAN in i.MX devices 

https://community.nxp.com/docs/DOC-1437 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

803 Views
zcx891106
Contributor I

Hi. I have a look at the flexcan clk source change on imx6ULLRM. But the FLEXCAN_CTRLX don't have the register on imx6ullRM. I also have a look at the imx25RM. The bit13 of the  FLEXCAN_CTRLX is the clk source change bit. So I don't know imx6ull can or not  select the clk source.

0 Kudos