I can set the max clock on MCIMXULL-EVK to 528MHz but not 792MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can set the max clock on MCIMXULL-EVK to 528MHz but not 792MHz

Jump to solution
1,035 Views
JohnKlug
Senior Contributor I

If I try to set the clock using Linux and the userspace governor, it will accept 528MHz, but anything higher skips to 900MHz:

root@imx6ullevk:/lib/modules# echo 500000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq
528000
root@imx6ullevk:/lib/modules# echo 530000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq
900000
root@imx6ullevk:/lib/modules# echo 792000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed                                                                        
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
userspace
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq
900000
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq                                                                                  
900000

 

What do I need to do to set the maximum clock to 792MHz?

root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor                                                                                  
userspace
0 Kudos
1 Solution
935 Views
dtony
Contributor III

I believe you need to check the scaling_available_frequencies to see how many opp the system have. 

cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies

you need to type 528000 to set the 528M,which should list in scaling_available_frequencies. 

The exact number in scaling_available_frequencies.

 

And I believe BSP code has problem. 

linux/drivers/cpufreq/imx6q-cpufreq.c

/*
* Speed GRADING[1:0] defines the max speed of ARM:
* 2b'00: Reserved;
* 2b'01: 528000000Hz;
* 2b'10: 696000000Hz on i.MX6UL, 792000000Hz on i.MX6ULL;
* 2b'11: 900000000Hz on i.MX6ULL only;
* We need to set the max speed of ARM according to fuse map.
*/
val >>= OCOTP_CFG3_SPEED_SHIFT;
val &= 0x3;

// now the val is 0x3.

//#define OCOTP_CFG3_6ULL_SPEED_792MHZ 0x2
//#define OCOTP_CFG3_6ULL_SPEED_900MHZ 0x3

//val != OCOTP_CFG3_6ULL_SPEED_792MHZ is wrong I believe.

//should be 

// if ((val != OCOTP_CFG3_6ULL_SPEED_792MHZ)&&(val != OCOTP_CFG3_6ULL_SPEED_900MH))

if (of_machine_is_compatible("fsl,imx6ull")) {
 if (val != OCOTP_CFG3_6ULL_SPEED_792MHZ)
if (dev_pm_opp_disable(dev, 792000000))
dev_warn(dev, "failed to disable 792MHz OPP\n");

if (val != OCOTP_CFG3_6ULL_SPEED_900MHZ)
if (dev_pm_opp_disable(dev, 900000000))
dev_warn(dev, "failed to disable 900MHz OPP\n");
}

return ret;
}

 

View solution in original post

0 Kudos
8 Replies
1,011 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Please provide your device tree and also the inputs on

cat /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state

Thank you

0 Kudos
1,006 Views
JohnKlug
Senior Contributor I

cat /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state
198000 0
396000 35418
528000 0
900000 0

Since this is the NXP EVK board, I have made no changes to the device tree.

How do I provide device tree source?  I could do a reverse compile.

 

I am using 5.15.71:

95448dd0dc9b621ae027cbefedaaa7c3d0d3ad2d
(tag: lf-5.15.71-2.2.0, origin/lf-5.15.y

5.15.y imx6ull device tree root 

I gzipped the dtb file.

0 Kudos
968 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

I understand that it's working from you created case, please refer to IMX REFERENCE MANUAL page 33.

If the frequency is not defined in DTS, the CPUFREQ driver changes the CPU frequency
to the nearest higher frequency in the array.

The initial clock speed is 528 MHz, then you change it to 530 MHz, the nearest defined frequency is 900 Mhz, same for the other command.

What is really concerning is your reply, it doesn't get back to 528MHz.

To set the clock to 792 MHz you have to set up that option in the device tree, see the next example.

josephlinares_0-1681797638541.png

Thank you

0 Kudos
961 Views
JohnKlug
Senior Contributor I

It appears that 792000 is already defined in device tree in cpu0.

Here is the live device tree for imx6ull-14x14-evk:

root@imx6ullevk:/proc/device-tree/cpus/cpu@0# xxd -g4 fsl,soc-operating-points                                                                                                                                      
00000000: 000dbba0 001312d0 000c15c0 0011edd8  ................
00000010: 00080e80 0011edd8 00060ae0 0011edd8  ................
00000020: 00030570 0011edd8                    ...p....
root@imx6ullevk:/proc/device-tree/cpus/cpu@0# xxd -g4 operating-points
00000000: 000dbba0 00137478 000c15c0 0012b128  ......tx.......(
00000010: 00080e80 0011edd8 00060ae0 000fa3e8  ................
00000020: 00030570 000e7ef0                    ...p..~.

0x000c15c0 =  792000
0x0011edd8 = 1175000
0x0012b128 = 1225000

Should I delete all the other operating points except 792000?

0 Kudos
958 Views
JohnKlug
Senior Contributor I

Additional information:

root@imx6ullevk:/sys/devices/system/cpu/cpufreq/policy0# echo 792000 >scaling_max_freq 
root@imx6ullevk:/sys/devices/system/cpu/cpufreq/policy0# cat scaling_max_freq 
528000
0 Kudos
1,026 Views
JohnKlug
Senior Contributor I

Now it won't even set the 528MHz:

root@imx6ullevk:/lib/modules# echo 500000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq  
900000
root@imx6ullevk:/lib/modules# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor                                                                                  
userspace


So is something setting the clock speed for me?

0 Kudos
936 Views
dtony
Contributor III

I believe you need to check the scaling_available_frequencies to see how many opp the system have. 

cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies

you need to type 528000 to set the 528M,which should list in scaling_available_frequencies. 

The exact number in scaling_available_frequencies.

 

And I believe BSP code has problem. 

linux/drivers/cpufreq/imx6q-cpufreq.c

/*
* Speed GRADING[1:0] defines the max speed of ARM:
* 2b'00: Reserved;
* 2b'01: 528000000Hz;
* 2b'10: 696000000Hz on i.MX6UL, 792000000Hz on i.MX6ULL;
* 2b'11: 900000000Hz on i.MX6ULL only;
* We need to set the max speed of ARM according to fuse map.
*/
val >>= OCOTP_CFG3_SPEED_SHIFT;
val &= 0x3;

// now the val is 0x3.

//#define OCOTP_CFG3_6ULL_SPEED_792MHZ 0x2
//#define OCOTP_CFG3_6ULL_SPEED_900MHZ 0x3

//val != OCOTP_CFG3_6ULL_SPEED_792MHZ is wrong I believe.

//should be 

// if ((val != OCOTP_CFG3_6ULL_SPEED_792MHZ)&&(val != OCOTP_CFG3_6ULL_SPEED_900MH))

if (of_machine_is_compatible("fsl,imx6ull")) {
 if (val != OCOTP_CFG3_6ULL_SPEED_792MHZ)
if (dev_pm_opp_disable(dev, 792000000))
dev_warn(dev, "failed to disable 792MHz OPP\n");

if (val != OCOTP_CFG3_6ULL_SPEED_900MHZ)
if (dev_pm_opp_disable(dev, 900000000))
dev_warn(dev, "failed to disable 900MHz OPP\n");
}

return ret;
}

 

0 Kudos
924 Views
JohnKlug
Senior Contributor I

With a patch, it will now run at 792MHz.  So this does appear to be a bug in the clock driver code.

I made a patch for anyone who happens to read this.

0 Kudos