I.Mx8mmini :LIBUSB_ERROR_TIMEOUT ] SDPU: write -f imx-boot-imx8mmevk-s

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.Mx8mmini :LIBUSB_ERROR_TIMEOUT ] SDPU: write -f imx-boot-imx8mmevk-s

4,234 次查看
santhosh2
Contributor IV

Hi,

We are flashing our new i.mx8mmini PCB board and we are getting the error as below while flashing
---------------------------------------------------------------------------------------------------------
Success 0    Failure 1                                                        
                                                                               
1:13   2/ 3   [HID(W):LIBUSB_ERROR_TIMEOUT ] SDPU: write -f imx-boot-imx8mmevk-s
-----------------------------------------------------------------------------------------------------------
debug port trace Log is attached and uuu error screen shot is also attached for your quick reference 
Kindly let us know what may be the root cause of the above said error
LIBUSB_ERROR_TIMEOUT.png
0 项奖励
1 回复

3,946 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

one can look at answer on

Flashing iMX8MM-EVK using UUU Tool on Ubuntu 

issue with flashing Universal update utility for iMX8MQ · Issue #91 · NXPmicro/mfgtools · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励