I.MX6ULL minicom USB connecting problem(ttyUSB0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6ULL minicom USB connecting problem(ttyUSB0)

424件の閲覧回数
kzy545
Contributor I

Hellow

I'm trying to use I.MX6ULL but i have a problem of minicom

222.png

It is i connected board with SD card which has booting image

And than i run minicom and do setting like that

3333.png

after setting i did run minicom again to connect with my board but when i run minicom i could not connect with my board like that

4444.png111.PNG

Also, i could not find 'ttyUSB0' in the /dev

Now, i am expecting SD card doesn't have exact booting image or use another USB Port

Could you hele me sort my problem out?

ラベル(2)
0 件の賞賛
1 返信

295件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi Shinbok KIM,

Hope you have connected USB Debug cable to J1901 on the base board (mentioned in Quick start Guide for imx6ULL).