I.MX6SoloX2 - Linux 5.4.70_2.3.0 - Kernel hangs while booting without any error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6SoloX2 - Linux 5.4.70_2.3.0 - Kernel hangs while booting without any error

Jump to solution
3,164 Views
parth_shah
Contributor III

Hello folks,

I have been using Linux 4.14.238 version for I.MX6SoloX2 SOM without any issues. Due dependency of custom network switch driver which is supported on Linux 5.4, I have to move the Linux kernel version from 4.14 to 5.4

I am using NXP release of 5.4.70_2.3.0 supported for i.MX6SoloX Processor. I am able to successfully compile the compile the packages. 

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus

But When the Board boots up, without showing any error kernel hangs indefinitely after loading ahci (SATA) driver.

I checked imx6sx.dtsi file for both linux versions and could not find major difference which could lead to this error. I have been using default kernel configuration imx_v7_defconfig.

Can anyone please share their opinion what could be reason of this error?

## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-5.4.70+g05ce692fbc29
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 9015880 Bytes = 8.6 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 81000000
Booting using the fdt blob at 0x81000000
Loading Kernel Image ... OK
Loading Device Tree to 9df1b000, end 9df28e0e ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.70+g05ce692fbc29 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Wed Dec 16 05:31:24 UTC 2020
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Freescale i.MX6 SoloX SG base Board
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] Reserved memory: created CMA memory pool at 0x88000000, size 320 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] percpu: Embedded 15 pages/cpu s31244 r8192 d22004 u61440
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129666
[ 0.000000] Kernel command line: console=ttymxc0,115200 ubootver=2016.03-g25d39d31-g7969642 root=/dev/mmcblk3p2 rw rootfstype=ext4
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 171316K/523264K available (11264K kernel code, 533K rwdata, 4464K rodata, 1024K init, 435K bss, 24268K reserved, 327680K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76430001
[ 0.000000] random: get_random_bytes called from start_kernel+0x2c8/0x488 with crng_init=0
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.000032] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.001468] Console: colour dummy device 80x30
[ 0.001496] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.001511] pid_max: default: 32768 minimum: 301
[ 0.001664] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.001678] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.002424] CPU: Testing write buffer coherency: ok
[ 0.002467] CPU0: Spectre v2: using BPIALL workaround
[ 0.002756] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.003352] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.003524] rcu: Hierarchical SRCU implementation.
[ 0.003814] smp: Bringing up secondary CPUs ...
[ 0.003826] smp: Brought up 1 node, 1 CPU
[ 0.003835] SMP: Total of 1 processors activated (6.00 BogoMIPS).
[ 0.003842] CPU: All CPU(s) started in SVC mode.
[ 0.004220] devtmpfs: initialized
[ 0.009535] Duplicate name in lcdif@2224000, renamed to "display#1"
[ 0.011327] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.011727] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.011750] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[ 0.032371] pinctrl core: initialized pinctrl subsystem
[ 0.033385] NET: Registered protocol family 16
[ 0.040160] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.049611] vdd1p1: supplied by regulator-dummy
[ 0.050169] vdd3p0: supplied by regulator-dummy
[ 0.050782] vdd2p5: supplied by regulator-dummy
[ 0.051323] vddarm: supplied by regulator-dummy
[ 0.051893] vddpcie: supplied by regulator-dummy
[ 0.052430] vddsoc: supplied by regulator-dummy
[ 0.053099] mxs_phy 20c9000.usbphy: 20c9000.usbphy supply phy-3p0 not found, using dummy regulator
[ 0.053623] mxs_phy 20ca000.usbphy: 20ca000.usbphy supply phy-3p0 not found, using dummy regulator
[ 0.067235] No ATAGs?
[ 0.067299] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.067313] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.069596] imx6sx-pinctrl 20e0000.iomuxc: Invalid fsl,pins or pins property in node /soc/aips-bus@2000000/iomuxc@20e0000/imx6x-sg/pciereggrp
[ 0.069686] imx6sx-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.072084] imx mu driver is registered.
[ 0.073071] imx rpmsg driver is registered.
[ 0.074379] MU is ready for cross core communication!
[ 0.103077] vgaarb: loaded
[ 0.103939] SCSI subsystem initialized
[ 0.104442] usbcore: registered new interface driver usbfs
[ 0.104495] usbcore: registered new interface driver hub
[ 0.104581] usbcore: registered new device driver usb
[ 0.104752] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[ 0.106392] i2c i2c-0: IMX I2C adapter registered
[ 0.107320] i2c i2c-1: IMX I2C adapter registered
[ 0.108083] pca953x 2-0020: using no AI
[ 0.131682] pca953x 2-0021: using no AI
[ 0.140833] pca953x 2-0021: failed writing register
[ 0.140989] i2c i2c-2: IMX I2C adapter registered
[ 0.141869] i2c i2c-3: IMX I2C adapter registered
[ 0.142394] mc: Linux media interface: v0.10
[ 0.142446] videodev: Linux video capture interface: v2.00
[ 0.142500] pps_core: LinuxPPS API ver. 1 registered
[ 0.142509] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.142529] PTP clock support registered
[ 0.170784] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 0.172291] MIPI CSI2 driver module loaded
[ 0.172346] Advanced Linux Sound Architecture Driver Initialized.
[ 0.173521] Bluetooth: Core ver 2.22
[ 0.173580] NET: Registered protocol family 31
[ 0.173589] Bluetooth: HCI device and connection manager initialized
[ 0.173606] Bluetooth: HCI socket layer initialized
[ 0.173616] Bluetooth: L2CAP socket layer initialized
[ 0.173641] Bluetooth: SCO socket layer initialized
[ 0.174252] clocksource: Switched to clocksource mxc_timer1
[ 0.174435] VFS: Disk quotas dquot_6.6.0
[ 0.174521] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.183743] thermal_sys: Registered thermal governor 'step_wise'
[ 0.184070] NET: Registered protocol family 2
[ 0.184729] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[ 0.184769] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear)
[ 0.184815] TCP bind hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.184882] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.184978] UDP hash table entries: 256 (order: 1, 8192 bytes, linear)
[ 0.185007] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear)
[ 0.185210] NET: Registered protocol family 1
[ 0.185773] RPC: Registered named UNIX socket transport module.
[ 0.185786] RPC: Registered udp transport module.
[ 0.185793] RPC: Registered tcp transport module.
[ 0.185801] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.186339] PCI: CLS 0 bytes, default 64
[ 0.186996] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 0.188716] Bus freq driver module loaded
[ 0.189728] Initialise system trusted keyrings
[ 0.189955] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.196323] NFS: Registering the id_resolver key type
[ 0.196354] Key type id_resolver registered
[ 0.196362] Key type id_legacy registered
[ 0.196407] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.196911] fuse: init (API version 7.31)
[ 0.232248] Key type asymmetric registered
[ 0.232262] Asymmetric key parser 'x509' registered
[ 0.232285] io scheduler mq-deadline registered
[ 0.232293] io scheduler kyber registered
[ 0.247385] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
[ 0.247403] imx-sdma 20ec000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx6q.bin
[ 0.249447] mxs-dma 1804000.dma-apbh: initialized
[ 0.256721] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 24, base_baud = 5000000) is a IMX
[ 1.043776] printk: console [ttymxc0] enabled
[ 1.049225] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 68, base_baud = 5000000) is a IMX
[ 1.058813] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 69, base_baud = 5000000) is a IMX
[ 1.068304] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 70, base_baud = 5000000) is a IMX
[ 1.077769] 21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 71, base_baud = 5000000) is a IMX
[ 1.087265] 22a0000.serial: ttymxc5 at MMIO 0x22a0000 (irq = 83, base_baud = 5000000) is a IMX
[ 1.098050] imx sema4 driver is registered.
[ 1.119720] brd: module loaded
[ 1.131392] loop: module loaded
[ 1.135889] at24 1-0052: 4096 byte 24c32 EEPROM, writable, 32 bytes/write
[ 1.144203] imx ahci driver is registered.

 

 

 

 

Labels (3)
0 Kudos
1 Solution
3,064 Views
parth_shah
Contributor III

In dts node, I set the SPI max Frequency as 40 MHz(spi-max-frequency = <40000000>). Due to some change in the driver, it gets multiplied with 4, hence SPI frequency becomes 160MHz. 

So, setting SPI max frequency as 10 MHz (spi-max-frequency = <10000000>) solves the problem.

View solution in original post

0 Kudos
8 Replies
3,065 Views
parth_shah
Contributor III

In dts node, I set the SPI max Frequency as 40 MHz(spi-max-frequency = <40000000>). Due to some change in the driver, it gets multiplied with 4, hence SPI frequency becomes 160MHz. 

So, setting SPI max frequency as 10 MHz (spi-max-frequency = <10000000>) solves the problem.

0 Kudos
3,143 Views
igorpadykov
NXP Employee
NXP Employee

Hi Parth

 

one can check if proper uboot version was used for Linux 5.4.70_2.3.0  :

https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=imx_v2020.04_5.4.70_2.3.0

also one can try to decrease cma size

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sx.dtsi?h=imx_5.4.70...

 

Best regards
igor

0 Kudos
3,133 Views
parth_shah
Contributor III

I found out that it gets stuck because of QSPI node.

&qspi2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_qspi2>;
status = "okay";
ddrsmp=<0>; //or 2

flash0: w25q128@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "winbond,w25q128", "jedec,spi-nor";
m25p,fast-read;
spi-max-frequency = <40000000>;
reg = <0>;
};
};

If I disable this node, kernel boots, but it gets stuck elsewhere.

Could you please check if configuration is proper or not?

0 Kudos
3,129 Views
igorpadykov
NXP Employee
NXP Employee

>Could you please check if configuration is proper or not?

 

one can look at nxp official imx_v2020.04_5.4.70_2.3.0 uboot

https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/dts/imx6sx-sdb.dts?h=imx_v2020.04...

 

Best regards
igor

0 Kudos
3,111 Views
parth_shah
Contributor III

I have same dts entry, still does not bootup

0 Kudos
3,109 Views
igorpadykov
NXP Employee
NXP Employee

are you using imx_v2020.04_5.4.70_2.3.0 or other ?

 

Best regards
igor

 

 

0 Kudos
3,100 Views
parth_shah
Contributor III

Yes, I am using  imx_v2020.04_5.4.70_2.3.0 for i.MX6SoloX2

0 Kudos
3,096 Views
igorpadykov
NXP Employee
NXP Employee

one can try to debug it and try to find reason for halt using  AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf

 

Best regards
igor

0 Kudos