I.MX6Q DDR stress test!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q DDR stress test!

2,114 Views
tommyduan
Contributor III

We test IMX6Q CPU  2GB DDR3  test DDR!we use test app V2.1 is OK,but when we use V2.9 or V3.0 is fail! we use the same .inc configuration files,What could be the reason?

the fail log:


============================================
DDR Stress Test (2.9.2)
Build: Sep 17 2018, 23:07:26
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO1.5
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00000000
SRC_SBMR2(0x020d801c) = 0x20000001
============================================

ARM Clock set to 1GHz

============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 15, col size: 10
Chip select CSD0 is used
Density per chip select: 2048MB
============================================


DDR Stress Test Iteration 1
Current Temperature: 54
============================================

DDR Freq: 352 MHz
t0.1: data is addr test
Address of failure(step2): 0x100032c4
Data was: 0x100032cc
But pattern should match address
Error: failed to run stress test!!!

Labels (2)
0 Kudos
8 Replies

1,780 Views
igorpadykov
NXP Employee
NXP Employee

Hi tommy

reason may be old .inc configuration files, recommended to use ones

provided with ddr tester with custom board modifications and use latest

i.MX6DQSDL DDR3 Script Aid

i.MX6ULL_LPDDR2_Script_Aid 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,780 Views
tommyduan
Contributor III

if we use V2.1 test !Whether the test data is affected?

0 Kudos

1,780 Views
igorpadykov
NXP Employee
NXP Employee

recommended to use latest version of ddr test.

0 Kudos

1,780 Views
tommyduan
Contributor III

I use the latest version,but  I find the error;What's wrong with the configuration?

微信图片_20190311103247.png

截图00.jpg

0 Kudos

1,780 Views
igorpadykov
NXP Employee
NXP Employee

one can look at below presentation describing its usage

DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations 

Best regards
igor

0 Kudos

1,780 Views
tommyduan
Contributor III

     Thanks for your reply!But I download V3.0 versions,Use the latest .inc configuration files!The following error will occur:ERROR: DCD addr is out of valid range.If we remove this command://setmem /16 0x020bc000 = 0x30,we can download .inc files!The following error occurs when I start running:

DDR Freq: 352 MHz
t0.1: data is addr test
t0: memcpy10 SSN x64 test
t1: memcpy8 SSN x64 test
t2: byte-wise SSN x64 test
t3: memcpy11 random pattern test
test2 Address: 0x4f2127c4
Data initally read was: 0xcc12da58
Data re-read is: 0xcc12da58
But pattern was: 0xcc12da48
Bit location: 0x00000010
Error: failed to run stress test!!!

we use V2.9 and V3.0 the same question!What went wrong here?

0 Kudos

1,780 Views
igorpadykov
NXP Employee
NXP Employee

this error is described in FAQ section of link

i.MX6/7 DDR Stress Test Tool V3.00 

Best regards
igor

0 Kudos

1,780 Views
tommyduan
Contributor III

Can you provide me the lastest version .inc Profile template?

0 Kudos