I.MX53 MT41J256M16-125:E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX53 MT41J256M16-125:E

1,023 Views
RuiBastos
Contributor II

Hi all,

Freescale IMX53 reference boards uses four MT41J128M16HA DDR3 (2Gbits 128X16) chips to achive 1GByte of memory.

Can I use only two MT41J256M16HA DDR3 (4Gbits 256X16) to achive the same 1GByte of memory ?

The idea is to reduce board size and routing.

has anyone tried this approach ? Anyone see any problems in this approach ?

thanks

Labels (1)
0 Kudos
3 Replies

587 Views
OlegGubaidullin
Contributor I

Hi,
I'm working on i.mx53 project with 4Gbit DDR3 chips and I've seen your post about these chips on imxcommunity forum.
Could you tell me please what changes you made in programming memory controller registers in compare to reference board.

0 Kudos

587 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi,

 

Yes. As long as the addressable space is less than 1GB per chip select and the number of bits is still 16, you can use it for your design.

 

Best regards.

Jorge.

0 Kudos

587 Views
kamejoko80
Contributor II

Hello,

I have the same problem. did you resolve this ?

0 Kudos