I.MX 6( MCIMX6S5EVM10ADR) BPM Microsystem programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX 6( MCIMX6S5EVM10ADR) BPM Microsystem programming

1,067 次查看
marco_villasana
Contributor I

Good afternoon, we are using the I.MX 6 in some of our products, we are currently using the NXP Mfg tool to program this device on board. We are willing to move this programing to a device level, prior to mounted on PCB, is it possible to program this micro using a programmer? (BPM machine in this case)

标签 (1)
0 项奖励
回复
6 回复数

1,012 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Marco

i.MX6 have not internal program flash, they use external media like

sd, or nor which may be programmed using programmer.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,012 次查看
marco_villasana
Contributor I

Thank you for your answer What about IMX8?

Regards!

0 项奖励
回复

1,012 次查看
igorpadykov
NXP Employee
NXP Employee

it is the same

Best regards
igor

0 项奖励
回复

1,012 次查看
marco_villasana
Contributor I

Thank you for the quick answer, so, just to be clear, the IMX6 and IMX8 can not be programmed using any kind of programmer right?

0 项奖励
回复

1,012 次查看
igorpadykov
NXP Employee
NXP Employee

right.

0 项奖励
回复

1,012 次查看
marco_villasana
Contributor I

Thanks for your attention

0 项奖励
回复