How to use "pcie EC and RC verify system"?

cancel
Showing results for 
Search instead for 
Did you mean: 

How to use "pcie EC and RC verify system"?

718 Views
mingmingyuan
Contributor III

dear freescal:

I want to verify my pcie bus, but I don't know how to connect two board.

Labels (3)
0 Kudos
3 Replies

444 Views
mingmingyuan
Contributor III

dear sir:

I have readed this link https://community.freescale.com/docs/DOC-95014

fsl's link description as blow:

Connected by 2*mini_PCIe to standard_PCIe  adaptors, 2*PEX cable adaptors,  and one PCIe cable.

my question is:

1,"mini_PCIe to standard_PCIe  adaptors" is  what? where can I got it?

2,"PEX cable adaptors" is what? where can I got it?

0 Kudos

444 Views
igorpadykov
NXP TechSupport
NXP TechSupport

HI mingmin

you should by these two cards

PM2C V2.1 (PCI-E / Mini PCI-E adapter)

then manually solder sata cable between them

please read carefully 'How to make it"

i.MX6Q PCIe EP/RC Validation System

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

444 Views
mingmingyuan
Contributor III

dear sir:

I have build image and flash image to EP board and RC board.

when system boot, I also look the log as below, so I think pcie link is OK.

but when I test send and receive data, result is fail. can you help me?

my test cmd:

EP side:

root@freescale /unit_tests$ ./memtool  -32 01000000=deadbeaf

Writing 32-bit value 0xDEADBEAF to address 0x01000000

RC side:

root@freescale /unit_tests$ ./memtool  -32 40000000 10

E

Reading 0x10 count starting at address 0x40000000

0x40000000:  DFFBFF4B DFFE3E75 7FF8FBFF 7FDBFEDD

0x40000010:  FEDA7DFA 7FFF58FF FF2DFEDA 5FDD3CFD

0x40000020:  F9F0FCBF 7FADADE7 EFF7FDEC FF797FED

0x40000030:  FDF3FFFD 7E8DEDEF FB077D2D BFFDF8FD

boot log:

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

PCIE: imx_pcie_pltfm_probe start link up.

IMX PCIe port: link up.

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff 64bit pref]

pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff 64bit pref] (PCI address [0x1000000-0x10fffff])

pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01-01]

pci 0000:00:00.0:   bridge window [io  disabled]

pci 0000:00:00.0:   bridge window [mem disabled]

pci 0000:00:00.0:   bridge window [mem pref disabled]

PCI: enabling device 0000:00:00.0 (0000 -> 0003)

0 Kudos