How to enable the USB TTY in the SABRE tablet iMX53?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable the USB TTY in the SABRE tablet iMX53?

1,272件の閲覧回数
mikedwn
Contributor II

Hello:

I am trying to setup Android Image to have the USB TTY driver. By using the menuconfig, the menu "Device Drivers" -> "USB support" -> "USB Serial Converter support" -> "USB Generic Serial Driver". Save the menuconfig, and build the kernel_imx. I modified the init.rc to add "chmod 0777 /dev/ttyACM*" to change mode. I flash to Android image into Sabre tablet, and power it up. I plug USB cable from the Sabre tablet into Kenetic ARM tower. But I don't see Android enum the USB device.

 

Can anyone who know how to setup Sabre Tablet to support USB TTY?

 

Thank You

Mike

タグ(2)
0 件の賞賛
4 返答(返信)

585件の閲覧回数
mikedwn
Contributor II

Yes, I anble the USB / Serial General Conversion. I did follow the Freescale Power Point that setup Android USB/Serial COM ("ttyACM0").

 

I am using the USB host connector. The Android is USB Host, and the K53 Kinitic is the device.

 

Mike

0 件の賞賛

585件の閲覧回数
mbp
Contributor V

Did you manage to get it running?

A brief list of steps you took would be MIGHTY helpful & appreciated!   :smileyhappy:

mike

0 件の賞賛

585件の閲覧回数
handala
Contributor I

Hello,

I'm facing the same issue. Can you please let me knos if you have solved it and how? Actually I can see ttyGS0,1,2,3 in /dev/ but when connecting my USB to the pc I don't see any enumeration happening.

Best regards,

Handala

0 件の賞賛

585件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I don´t know how to set up USB TTY, bu tit looks like you´re doing the right way (enabling it on kernel).

Are you using the right USB connector (host/otg)?????

0 件の賞賛