Hello,
What are the correct commands and procedure to enable the board's physical HDMI output using NXP's Android Automotive OS 12 prebuilt demo images using the i.MX 8QuadMax MEK? I would prefer not using the bulkier, LVDS to HDMI dongle during development.
In a previous, older v10 solution, I read to append these commands to uuu tool:
To test physical HDMI display, execute the tool with -u hdmi -d hdmi. HDMI_TX port is used for display
Another similar looking post says:
one can try vbmeta-imx8qm-hdmi.img image (image for i.MX 8QuadMax MEK board to support
physical HDMI display).
However in the "Rev. automotive-12.0.0_2.1.0 —1 September 2022 Android_Auto_User's_Guide.pdf" there is no file named "vbmeta-imx8qm-hdmi.img" listed... Section 8.3.3 states: To evaluate the multiple-display feature with physical HDMI on i.MX 8QuadMax MEK,
flash dtbo-imx8qm-md.img. Is flashing the *-md.img files all that's needed? If so, what uuu command is suggested?
Thanks.
Solved! Go to Solution.
To test multiple displays on i.MX 8QuadMax MEK with images in automotive-12.0.0_2.1.0_image_8qmek_car2.tar.gz, execute the tool with -u md -d md
so pls try to use "-u md and -d md" to test
To test multiple displays on i.MX 8QuadMax MEK with images in automotive-12.0.0_2.1.0_image_8qmek_car2.tar.gz, execute the tool with -u md -d md
so pls try to use "-u md and -d md" to test