How to designs without direct physical access to the SDP port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to designs without direct physical access to the SDP port

391 Views
dengboping
Contributor I

I meet SDP problem on 1.2G CPU IMX6Q . In ERR010872 :

How to designs without direct physical access to the SDP port?   It's USB port, add a buffer ?

"A specific mechanism is required to switch the target device into Serial Downloader
mode, in which the SDP can run. NXP can provide details of the mechanism and
guidance on methods and techniques to avoid it"

    what's the "specific mechanism"  ?

   Thanks!

Labels (1)
0 Kudos
1 Reply

328 Views
igorpadykov
NXP Employee
NXP Employee

Hi deng

there is new fuse SDP_DISABLE described in

Chapter 5 Fusemap i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
In general for security related questions recommended to use service request

as this may contain cofidential info.

https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos