How to calculate real time consumption for the I.MX6Q OpenCL kernels running on GPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to calculate real time consumption for the I.MX6Q OpenCL kernels running on GPU

770件の閲覧回数
haitaodeng
Contributor I

Hello everybody:

Our board is based on SabreLite(i.mx6q), using Linux3.10.

We use the GPU(gc2000) inside i.MX6Q with OpenCL to do some image processing.

Are there any methods to test the real processing time, when running the I.MX6Q OpenCL kernels.

So that we can know that how long does it take a OpenCL-kernel to run on GPU.

By the way, could you tell us where can we find the latest GPU driver for SabreLite(i.mx6q) and how to configure the GPU driver.

Thanks for your time.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

606件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Haitao

I believe this could be estimated with profiling tools like

IMX6 Memory Bandwidth usage - RidgeRun Developer Connection

also for latest 3.14.38 drivers one can look at

http://boundarydevices.com/nitrogen6_max-with-i-mx6-quad-plus-processor/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信