Hello, NXP Technical Support
I use the IMX8MP platform. I downloaded imx-6.1.36-2.1.0_desktop.xml from https://github.com/nxp-imx/imx-manifest to compile the desktop file system. How do I add qt, and How can I compile the SDK so that I can use qt
Here is the yocto command I am using now
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0_desktop.xml
DISTRO=imx-desktop-xwayland MACHINE=imx8mpevk source imx-setup-desktop.sh -b build-desktop
bitbake imx-image-desktop
Hi @xueyf
Modify below file: https://github.com/nxp-imx/meta-nxp-desktop/blob/lf-6.1.36-2.1.0-mickledore/recipes-fsl/images/imx-i...
Add inherit populate_sdk_qt6 in line 9 and then insert packagegroup-qt6-imx to IMAGE_INSTALL +=
Best Regards
Zhiming
Please add nxp-demo-experience in the bb file
When I use this method, the following error occurs. How should I solve it?
How to compile qt5 using yocto