How can I route audio from one sai to another?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I route audio from one sai to another?

980件の閲覧回数
venkatesh_selva
Contributor II

Hello all,

I streaming in HDMI-Input audio through sai5 and HDMI output using sai4 in iMX8MQ. How to route audio input from sai5 to sai4?

HDMI input is from Laptop HDMI output. HDMI output from imx8m to external monitor with speaker.

Using Android 8.1.0 in iMX8MQ.

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

845件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi venkatesh

data from one sai to another can be done with external connections

since there is no muxing capabilities, as for example in i.MX6DQ AUDMUX module.

Best regards
igor

0 件の賞賛
返信

845件の閲覧回数
venkatesh_selva
Contributor II

Unfortunately SAI4 is not an external one. Checked in EVK schematic also. Is it feasible by software?

Screenshot from 2019-07-04 13_22_27.png

0 件の賞賛
返信

845件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi venkatesh

 

for sai4 muxing options one can look sect.8.2 IOMUX Controller (IOMUXC)
0 件の賞賛
返信