Hi,
we have deployed Android 4.3 from Freescale on a Sabre DL. Now we are facing problems to get IPs on ethernet using DHCP or even statically set IPs.
Using DHCP we get the following:
30|root@tcandroid:/ # dhcpcd eth0
dhcpcd[3421]: flock `/data/misc/dhcp/dhcpcd-eth0.pid': Try again
1|root@tcandroid:/ # dhcpcd eth0
dhcpcd[3423]: version 5.5.6 starting
dhcpcd[3423]: eth0: checking for 169.254.85.56
dhcpcd[3423]: eth0: using IPv4LL address 169.254.85.56
dhcpcd[3423]: forked to background, child pid 3448
Which is wrong since it is getting a link-local address.
Setting a static IP we can set it but we cannot ping anything on the network:
ifconfig eth0 192.168.1.12
route add default dev eth0
ping 192.168.1.1
Getting:
PING 192.168.1.1 (192.168.1.1) 56(84) bytes of data.
From 192.168.1.177: icmp_seq=1 Destination Host Unreachable
From 192.168.1.177: icmp_seq=2 Destination Host Unreachable
From 192.168.1.177: icmp_seq=3 Destination Host Unreachable
From 192.168.1.177: icmp_seq=5 Destination Host Unreachable
From 192.168.1.177: icmp_seq=6 Destination Host Unreachable
It works fine with a Linux deployed (Debian kernel 3.0.35), so hardware is not the issue.
Any suggestions on how to further debug it?
已解决! 转到解答。
Hi Thomas,
actually we had a problem on the eMMC communication that was not using its full speed. So reducing the emmc communication speed, it was also limiting the Ethernet speed. Similarly to what you have suggested.
We have fixed the emmc communication bus and now we can get full gigabit ethernet.
Hello Rafael,
So you do not have internet at all correct?.. are you behind a proxy? ... android is pretty straightforward on this, you shouldn't have any problems right after plugging the ethernet cable.
Any messages on the terminal window?
Hi Thomas,
actually we had a problem on the eMMC communication that was not using its full speed. So reducing the emmc communication speed, it was also limiting the Ethernet speed. Similarly to what you have suggested.
We have fixed the emmc communication bus and now we can get full gigabit ethernet.
I had trouble with networking if the clock/cpu_freq was set too low in Debian. You have a lot of options for setting via Debian. You can use cpufreq-info/set in Debian to check which freq and CPU governor is being used.
I am not sure how Andriod sets it up, but you may want to check that. Andriod may be more low-power first, performance second.