HSIC I/F USB PHY information for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSIC I/F USB PHY information for i.MX6

Jump to solution
3,705 Views
yuuki
Senior Contributor II

Dear all,

We want to use USB Host port2 and Host port3 of i.MX6.

However, i.MX6 does not have Internal PHY for Host2 and Host3.

These Host ports are HSIC I/F and need external PHY.

Is there the HSIC I/F USB PHY with the operating experience?

Would you tell me a maker and the model number?

Is the sample driver for these PHY included in LinuxBSP?

(fsl-yocto-L3.14.52_1.1.0-ga.tar)

May I have advice?

Best Regards,

Yuuki

Labels (2)
Tags (3)
0 Kudos
1 Solution
1,126 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

SMSC USB4640 can be used and driver (..chipidea/usbmisc_imx.c,

..chipidea/ci_hdrc_imx.c) can be found in sources described in attached Linux Manual

Chapter 40 CHIPIDEA USB Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
1,127 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

SMSC USB4640 can be used and driver (..chipidea/usbmisc_imx.c,

..chipidea/ci_hdrc_imx.c) can be found in sources described in attached Linux Manual

Chapter 40 CHIPIDEA USB Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,126 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

Please tell me one more.

Is the sample driver of USB3503A included, too?

Is a driver modification necessary for USB3503A?

Best Regards,

Yuuki

0 Kudos
1,126 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

I am afraid not, sorry.

Best regards

igor