In one of our boards we use i.mx6-SOLOsabresd (MCIMX6S5EVM10AC) with Embedded Linux. Our current versions are:
In order to apply a certain feature we need to upgrade the BSP (Kernel, Linux,..). We tried:
Using the next images:
In all of the cases we encountered with the same problem – the GPU (Galcore.ko) is not working, we cannot run our graphic apps.
We need a solution for i.mx6-SOLOsabresd (MCIMX6S5EVM10AC).
Notes
Hello Noam,
For galcore you need to run the 5.0.11 version of the vivante driver and kernel 4.1.15, this don´t work for newer BSPs because NXP doesn´t have the MX6SoloSabreSD.
Regards
Dear Bio_TICFSL ,
For galcore you need to run the 5.0.11 version of the vivante driver and kernel 4.1.15
In order to apply certain things I need an updated BSP, the current version (4.1.15) does not help me.
NXP doesn´t have the MX6SoloSabreSD.
What does it means?