Hi,
I'm trying to configure an interrupt on a GPIO of my board i.MX6, in order to toggle another GPIO once the first has changed its value (this is the first stage of a more complicated project). I want to build a module and insert it on the running kernel. Attached is the source code and the Makefile I'm using to compile it. I'm actually able to compile the source code in a linux x86 system, but once I try to insert it on the i.MX6 environment (using insmod), I get these errors:
luca_gpio: Unknown symbol gpio_free (err 0)
luca_gpio: Unknown symbol __gpio_to_irq (err 0)
luca_gpio: Unknown symbol gpio_direction_output (err 0)
luca_gpio: Unknown symbol __gpio_set_value (err 0)
luca_gpio: Unknown symbol gpio_request (err 0)
Could anyone give me any suggestion to solve this issue, please?
Thanks a lot,
Luca
Original Attachment has been moved to: sources.zip
已解决! 转到解答。
Hello Luca,
I am trying to configure a GPIO pin and registered the ISR, (For more details please refer 474144). I have successfully registerd interrupt but my ISR is not getting hit.
Could you please share the DTS changes you have done and also updated source code, so that it will be helpful for us to resolve this issue.
Thanks,
Phani Movva
Hi Luca
I would suggest at below links for overview of i.MX6 gpio interrupt handling
Linux & GPIO userspace interrupts - Monocoques in Software
linux系统下标准GPIO按键驱动 - tiger_chen - 博客园
Best regards
igor
Hi Igor,
Thanks for your suggestions.
Actually I've already looked at the references you suggested and they have been very helpful as a start point. However, the method explained is working in polling mode and in user space: this means I'm not able to take a real-time action based on the state change of the input pin (e.g. change the state of another output pin). That's why I was asking about interrupts and kernel space modules. Any suggestion/explanation on how to achieve this?
Thanks guys,
Luca
Hi Igor,
Thanks for your suggestions. This is very interesting and a good starting point !
Just after having read the first pages, one more question is how to get all the starting point SW. I can download the 3.10.53 Linux kernel, but what about the BSP? And how should I combine the two software packages to get the full features OS for my i.MX6 Solo board? And what about the RFS?
Thanks a lot,
Luca
Hi Luca
for SW starting point suggest to start with
https://community.freescale.com/docs/DOC-1616
Best regards
igor