Freescale: Why is the Bit Rate( and file size) for H264 encoded videos on Freescale iMX6 inversely proportional to the resolution of video?
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
I am trying to build a live video streaming embedded server on Freescale imx6 with Gstreamer and h264 codecs. The client(Linux PC) is connected via a wireless link that streams the video transmitted by the server.
Recently I performed some test to measure the average bitrate for a h264 encoded file on a Freescale imx6 processor. I used the GStreamer element 'testvideosrc', ran it for 60 seconds and encoded it using the gstreamer-imx plugins that utilizes the hardware encoder (h264) and saved the file, and calculated the bitrate. Following is the command :
timeout --signal=SIGINT 60s \
gst-launch-1.0 -ev videotestsrc pattern=18 ! \
video/x-raw,width=100,height=50,framerate=10/1 ! \
imxvpuenc_h264 bitrate=5 ! h264parse ! \
filesink location=60s.h264 && \
echo $(( $(stat --format=%s 60s.h264) / 60 * 8))
The test was performed at 10 fps for different resolutions, and the bitrates are as follows:
Resolution BitRate
100 x 50 ~120.3K
320 x 240 ~93.7K
640 x 480 ~52.7K
1280 x 960 ~32.3K
The bitrate I calculated was for the file transfer rate, that I require to transfer this wirelessly over the communication link.
I am trying to understand the behaviour of the H264 encoder, as to why the bitrate is inversely proportional to the increasing resolution sizes. I had hoped that with increasing resolutions, the bitrate will also increase and hence was opting for a lower resolution image, for streaming through the wireless link. Can anyone explain, why this behaviour exists with the h264 codedc? Or am I at fault in understanding the bitrate demand.
Here is the file-size of the encoded video file.
Resolution File size in bytes
100 x 50 3886780
320 x 240 704543
640 x 480 397098
1280 x 960 235108
Could anyone explain this behaviour?
Please address this question to the H264 encoder experts, who can explain this behaviour.
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
the bitrate you set is too small, do you know what the real frame rate is? pls check frame rate when you set the different resolution.
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
Any updates for this question?
Regards.
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello Joan,
Here are more numbers at different framerates:
at 30 fps
Resolution File size in bytes Bitrate
100 x 50 3474013 455.16K
320 x 240 692716 92.36K
640 x 480 397563 53.01K
1280 x 960 234252 31.23K
at 60 fps
Resolution File size in bytes Bitrate
100 x 50 3470160 425.43K
320 x 240 703225 93.76K
640 x 480 399125 53.216K
1280 x 960 233787 31.168K
I do not understand "the real frame rate". How do I check this?
Regards.