External watchdog module on I.MX7ULPEVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External watchdog module on I.MX7ULPEVK

Jump to solution
977 Views
Raxesh-Oriya
Contributor III

I read about EWM(External Watchdog Monitor) from data sheet but I do not see anything related to watchdog in design files of BB(SPF-29164_B1) and SOM(spf-29163_b2).

The question is, how can I make use of this module?

RaxeshOriya_0-1629196447183.png

Labels (3)
0 Kudos
1 Solution
948 Views
igorpadykov
NXP Employee
NXP Employee

>I do not see EVM_OUT_b at PTB0 in SOM design file..

 

one can look IMX7ULPRMB2_Rev0_IOMUX.xlsx included in attachment tab Adobe reader

i.MX7ULPRMB2: i.MX 7ULP Applications Processor Reference Manual for Silicon Revision B2

EVM_OUT_b is muxed on PTB0(ALT12), it is accessable from both A7 and M4.

For A7 access one can use approach as in i2c-rpmsg driver 

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/i2c/busses/i2c-rpmsg-imx.c?h=lf-5....

 

Best regards
igor

View solution in original post

0 Kudos
3 Replies
969 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raxesh

 

description can be found in Chapter 61 External Watchdog Monitor (EWM)

i.MX7ULPRMB2: i.MX 7ULP Applications Processor Reference Manual for Silicon Revision B2

EVM_OUT_b  PTB0(ALT12) can be found in SOM schematic spf-29163 p.17 P1B (DDR_SODIMM_EDGE

FINGERS)  MCIMX7ULP-EVK Design Files

Seems there is no driver in NXP BSPs, so one will have to write own one.

 

Best regards
igor

0 Kudos
958 Views
Raxesh-Oriya
Contributor III

Hi @igorpadykov 

I do not see EVM_OUT_b at PTB0 in SOM design file. If it all it is the there I can't use it with A7 core, correct? because PTA and PTB are for M4 core.

RaxeshOriya_0-1629254603578.png

0 Kudos
949 Views
igorpadykov
NXP Employee
NXP Employee

>I do not see EVM_OUT_b at PTB0 in SOM design file..

 

one can look IMX7ULPRMB2_Rev0_IOMUX.xlsx included in attachment tab Adobe reader

i.MX7ULPRMB2: i.MX 7ULP Applications Processor Reference Manual for Silicon Revision B2

EVM_OUT_b is muxed on PTB0(ALT12), it is accessable from both A7 and M4.

For A7 access one can use approach as in i2c-rpmsg driver 

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/i2c/busses/i2c-rpmsg-imx.c?h=lf-5....

 

Best regards
igor

0 Kudos