Ethernet fried on iMX51?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet fried on iMX51?

1,249 Views
belgianwaffle
Contributor II

Hi,

We have a system built around the iMX51 running Linux.

I was using the memtool utility to poke around some status registers when something crazy happened.

By mistake I added an extra character to the address when using memtool and memtool tried to read a memory address outside of the available address space, which then the system froze and rebooted.

After reboot I have no Ethernet. I tried checking the status of the FEC control register using memtool, but my system just freezes evereytime I access the entire FEC address space.

Also, during the boot sequence FEC is not loaded anymore. This leads me to believe it is fried.

So...is Ethernet totally shot on the iMX or is there anything else I can try?

Labels (2)
0 Kudos
Reply
3 Replies

1,117 Views
belgianwaffle
Contributor II

Hmm nobody? OK maybe people are unfamiliar with memtool. It's just a tool that let's you poke around memory addresses. I'm not sure why It broke Ethernet of all things, but that is not my concern at this time.

Anyway, my main question is about the Ethernet controller not working. Is it safe to assume that if it is not loading that it is fried?

Edit: I changed the title of the thread to something more straightforward.

0 Kudos
Reply

1,117 Views
YixingKong
Senior Contributor IV

Hi

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

1,117 Views
YixingKong
Senior Contributor IV

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos
Reply