Hi All.
I have a design where I need two displays (LVDS) output from the iMX6, together with two individual audio outputs (one for each display).
Is it possible to do this with the iMX6?
Can I have two codecs interfaced to the iMX6?
(As I read the manual there is only one I2S interface).
Do someone have a link to design implementing this?
BR
Martin.
Hi Martin
yes, this is possible, i.MX6DQ has three SSI modules.
I am not aware of such design, however one can look at attached
document Chapter 8 Porting Audio Codecs to a Custom Board,
describing adding new codec.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------