Does the Ethernet Controller on the i.MX 6Solo uses DMA?.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does the Ethernet Controller on the i.MX 6Solo uses DMA?.

跳至解决方案
682 次查看
andresgonzalez
Contributor II

Hi Freescale Community.

We are using the Ethernet Controller of i.MX 6Solo processor and we are not sure if this controller uses DMA in any way.

Could somebody please clarify me if DMA is used by this controller and the purpose of its usage?.

Thanks in advance.

P.D.: We are using the Legacy Buffer Descriptors.

标签 (3)
标记 (5)
1 解答
570 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andres

yes i.MX6S ENET module has own DMA engine - "uDMA", one

can find its references in particular in

IMX6SDLRM sect. 23.5.14.1 Enhanced receive buffer descriptor:

"This section discusses the enhanced uDMA receive buffer descriptor..."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
571 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andres

yes i.MX6S ENET module has own DMA engine - "uDMA", one

can find its references in particular in

IMX6SDLRM sect. 23.5.14.1 Enhanced receive buffer descriptor:

"This section discusses the enhanced uDMA receive buffer descriptor..."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

570 次查看
andresgonzalez
Contributor II

Thanks for your help.

0 项奖励