Does mx25 requires SwapBBI support in NAND driver?

取消
显示结果 
搜索替代 
您的意思是: 
已解决

Does mx25 requires SwapBBI support in NAND driver?

跳至解决方案
664 次查看
rohith1z
Contributor III

Hi,

I'm running a custom kernel on a custom board based on mx25.

It has a 2GB micron nand flash.(2k+64B spare)

Kernel is based freescale L2.6.28 release.

I became aware of  the SwapBBI issue/feature with the NFC(attached document), when investigating nand corruption issues.

The newer releases have a swap BBI feature in the mxc nand driver.

My query is: Is this applicable to MX25 so that I can back port the driver?

Obviously I would need to propagate the changes to boot loader and factory flash programmer.

In some forums, I read that it would be applicable to only imx31 and imx27 and hence the confusion.

标签 (3)
0 项奖励
1 解答
446 次查看
shaojun_wang
NXP Employee
NXP Employee

Yes, you can back port the swap bbi driver from newer bsp to older bsp, include kernel, uboot and factory flash programmer.

在原帖中查看解决方案

0 项奖励
1 回复
447 次查看
shaojun_wang
NXP Employee
NXP Employee

Yes, you can back port the swap bbi driver from newer bsp to older bsp, include kernel, uboot and factory flash programmer.

0 项奖励