Document problem about iMX6 Android patches

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Document problem about iMX6 Android patches

跳至解决方案
2,506 次查看
DeanHuang
Contributor III

Hi,

I have a imx6 android question.

In Android User Guide, writes:

Get R13.4-GA kernel source code from freescale's opensource git:

$ cd myandroid

$ git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx # the kernel repo is

heavy, so this can take a while

$ cd kernel_imx

$ git checkout imx-android-13.4.1


Does it mean that I do not need to do this in "Patch code for i.MX"

Assume you had unzipped i.MX Android release package to /opt/imx-android-13.4.1/.

$ cd ~/myandroid

$ source /opt/imx-android-13.4.1/code/13.4.1/and_patch.sh

$ help

Now you should see that the "c_patch" function is available

$ c_patch /opt/imx-android-13.4.1/code/13.4.1 imx_13.4.1


I just need to do this ?

If your software has upgraded to R13.4-GA and you would only like to apply the additional patches between R13.4-GA and

13.4.1, please use the following steps:

Take framwork/base.git as an example. Assume you had unzipped i.MX Android release package

to /opt/imx-android-13.4.1/ .

$ cd /opt/imx-android-13.4.1/code/13.4.1-delta/platform/frameworks/base.git

$ ls *.patch > series

$ cd ~/myandroid/frameworks/base

$ git quiltimport --patches /opt/imx-android-13.4.1/code/13.4.1-delta/platform/frameworks/

base.git

I just have some confuse.

Thanks!!

标签 (2)
1 解答
1,074 次查看
DeanHuang
Contributor III

Dears,

I had solved this problem. It should use "imx-android-13.4.1/code/13.4.1/" instead of "imx-android-13.4.1/code/13.4.1-delta".

But I still have one question:

When I compiling the source code, there are some error messages.

ex:

host C++: obbtool <= frameworks/base/tools/obbtool/Main.cpp
:0:0: error: “_FORTIFY_SOURCE” redefined [-Werror]
:0:0: note: this is the location of the previous definition
cc1plus: all warnings being treated as errors


or

ERROR:  frameworks/compile/slang/slang_rs_export_foreach.cpp:247:23:
error: variable ‘ParamName’ set but not used [-Werror=unused-but-set- variable]


I had building image successfully  by correcting source code. But I'm confused that these error are source code problem or compiling environment problem?

My environment is Ubuntu 12.04 64 bit.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,075 次查看
DeanHuang
Contributor III

Dears,

I had solved this problem. It should use "imx-android-13.4.1/code/13.4.1/" instead of "imx-android-13.4.1/code/13.4.1-delta".

But I still have one question:

When I compiling the source code, there are some error messages.

ex:

host C++: obbtool <= frameworks/base/tools/obbtool/Main.cpp
:0:0: error: “_FORTIFY_SOURCE” redefined [-Werror]
:0:0: note: this is the location of the previous definition
cc1plus: all warnings being treated as errors


or

ERROR:  frameworks/compile/slang/slang_rs_export_foreach.cpp:247:23:
error: variable ‘ParamName’ set but not used [-Werror=unused-but-set- variable]


I had building image successfully  by correcting source code. But I'm confused that these error are source code problem or compiling environment problem?

My environment is Ubuntu 12.04 64 bit.

0 项奖励
回复
1,074 次查看
LeonardoSandova
Specialist I

Hi Dean, it would be great if you post the patch with all the changes needed to compile android on your Ubuntu machine. About your question, I am not sure, but it may be the host system your are using to compile Android.

0 项奖励
回复
1,074 次查看
DeanHuang
Contributor III

Hi Leonardo,

These are the error messages and solutions I found from network. There may be other solutions.

My Environment:

Ubuntu 12.04 64 bit

imx-android-13.4.1.tar.gz

Sorry for that I forget what ubuntu packages I installed before building Android.

Q1

host C++: obbtool <= frameworks/base/tools/obbtool/Main.cpp
     :0:0: error: “_FORTIFY_SOURCE” redefined [-Werror]
     :0:0: note: this is the location of the previous definition
     cc1plus: all warnings being treated as errors

S1

To fix this, edit build/core/combo/HOST_linux-x86.mk and replace:
     HOST_GLOBAL_CFLAGS += -D_FORTIFY_SOURCE=0
with
     HOST_GLOBAL_CFLAGS += -U_FORTIFY_SOURCE -D_FORTIFY_SOURCE=0


Q2

ERROR:  frameworks/compile/slang/slang_rs_export_foreach.cpp:247:23:
error: variable ‘ParamName’ set but not used [-Werror=unused-but-set-
variable]

S2

android/ics/frameworks/compile/slang/Android.mk
-local_cflags_for_slang := -Wno-sign-promo -Wall -Wno-unused-parameter -Werror
+local_cflags_for_slang := -Wno-sign-promo -Wall -Wno-unused-parameter


Q3

external/mesa3d/src/glsl/linker.cpp: In function ‘void link_shaders(const gl_context*, gl_shader_program*)’:
external/mesa3d/src/glsl/linker.cpp:1734:49: error: expected primary-expression before ‘,’ token
external/mesa3d/src/glsl/linker.cpp:1734:50: error: ‘fragColor’ was not declared in this scope
external/mesa3d/src/glsl/linker.cpp:1734:59: error: ‘offsetof’ was not declared in this scope
make: *** [out/host/linux-x86/obj/STATIC_LIBRARIES/libMesa_intermediates/src/glsl/linker.o] Error 1

S3

Adding a "#include <stddef.h>" to linker.cpp


Q4

ERROR:  external/oprofile/libpp/format_output.h:94:22: error:
reference ‘counts’ cannot be declared ‘mutable’ [-fpermissive]

S4

external/oprofile/libpp/format_output.h
-               mutable counts_t & counts;
+               counts_t & counts;


Q5

android_repo/external/llvm/lib/Support/Mutex.cpp:69: undefined reference to `pthread_mutexattr_init'
android_repo/external/llvm/lib/Support/Mutex.cpp:75: undefined reference to `pthread_mutexattr_settype'
android_repo/external/llvm/lib/Support/Mutex.cpp:80: undefined reference to `pthread_mutexattr_setpshared'
android_repo/external/llvm/lib/Support/Mutex.cpp:89: undefined reference to `pthread_mutexattr_destroy'
out/host/linux-x86/obj/STATIC_LIBRARIES/libLLVMSupport_intermediates/libLLVMSupport.a(Mutex.o): In function `llvm::sys::MutexImpl::tryacquire()':
android_repo/external/llvm/lib/Support/Mutex.cpp:143: undefined reference to `pthread_mutex_trylock'
collect2: ld returned 1 exit status

S5

Way1:
system/extras/tests/bionic/libc/Android.mk
LOCAL_MODULE_TAGS := tests

-LOCAL_LDFLAGS := \
+LOCAL_LDLIBS := \
    -lpthread \
    -ldl

Way2:
external/llvm/llvm-host-build.mk
LOCAL_LDLIBS := -lpthread -ldl


Q6

external/gtest/src/../src/gtest-filepath.cc:180:28: warning: missing initializer for member ‘stat::st_dev’ [-Wmissing-field-initializers]

external/gtest/src/../src/gtest-filepath.cc:180:28: warning: missing initializer for member ‘stat::__pad1’ [-Wmissing-field-initializers]

...
...
...
external/gtest/src/../src/gtest-filepath.cc:208:28: warning: missing initializer for member ‘stat::st_ino’ [-Wmissing-field-initializers]
make: *** [out/host/linux-x86/obj/STATIC_LIBRARIES/libgtest_host_intermediates/gtest-all.o] Error 1

S6

external/gtest/include/gtest/internal/gtest-param-util.h
add
#include <cstddef>