Disable screen blanking on i.MX6 running Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable screen blanking on i.MX6 running Yocto

Jump to solution
10,616 Views
marlonsmith
Contributor IV

Hi everyone,

I'm running a Yocto build on an i.MX6 board and I'm trying to stop the screen from shutting off after 15 minutes of inactivity.  I've tried the following things with no success:

- passing consoleblank=0 to bootargs

- modifying drivers/tty/vt/vt.c with static int blankinterval = 0;

Neither of these has had any effect.

cat /sys/module/kernel/parameters/consoleblank returns a value of 900.

My system does not have setterm.

Please help!

Thanks

Marlon

Tags (2)
1 Solution
3,875 Views
Yuri
NXP Employee
NXP Employee

Marlon,


   Perhaps the problem concerns with the fact, that the mentioned command(s) should be

issued, when all Linux sub-systems are working.  As a solution, one can run (own) special

application (at start up), which should issue the command ("echo 0 > /sys/class/graphics/fb0/blank")

after some period of time (several munutes).

~Yuri.

View solution in original post

0 Kudos
7 Replies
3,875 Views
Yuri
NXP Employee
NXP Employee

Please try the following :

echo -e -n '\033[9]' > /dev/tty0

or

echo 0 > /sys/class/graphics/fbx/blank

fbx - is number of framebuffer (LCD, LVDS, HDMI), x =0,1,2


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,875 Views
marlonsmith
Contributor IV

Yuri, I've tried both of your suggestions and neither of them is working.  The screen still goes blank after 15 minutes.

Any other ideas?

Thanks!

Marlon

0 Kudos
3,875 Views
Yuri
NXP Employee
NXP Employee

  Please try using command  "echo 0 > /sys/class/graphics/fb0/blank" under root.

~Yuri.

0 Kudos
3,875 Views
marlonsmith
Contributor IV

Yuri, if I run that command after the screen has shut off, it does turn the screen back on.  So it seems I'm on the right track.  However when I run the command in a script on startup it does not seem to prevent the screen from blanking eventually.  Any thoughts?

0 Kudos
3,876 Views
Yuri
NXP Employee
NXP Employee

Marlon,


   Perhaps the problem concerns with the fact, that the mentioned command(s) should be

issued, when all Linux sub-systems are working.  As a solution, one can run (own) special

application (at start up), which should issue the command ("echo 0 > /sys/class/graphics/fb0/blank")

after some period of time (several munutes).

~Yuri.

0 Kudos
3,875 Views
marlonsmith
Contributor IV

Thanks for the help Yuri.  What finally solved the problem was calling

echo -e '\033[9;0]' > /dev/tty1

from within my application, which runs once the rest of the system has been started.

Marlon

0 Kudos
3,875 Views
marlonsmith
Contributor IV

Thanks for the response Yuri!

I forgot that I had also already tried echo 0 > /sys/class/graphics/fbx/blank, but I will try echo -e -n '\033[9]' > /dev/tty0 and see if that works.

0 Kudos