Hi,
I have read the document http://cache.freescale.com/files/32bit/doc/app_note/AN4686.pdf
For disabling JTAG permanently we need to make set this OTP SJC_DISABLE.
I found commands like "fuse prog 0 6 0x100000", but this will work in uboot.
I need a command to disable the JTAG after application startup.
Is /sys/fsl_otp/HW_OCOTP_CFG5 OTP is the one ??
What value we need to fuse ?
is echo 0x100000 > /sys/fsl_otp/HW_OCOTP_CFG5 is same as fuse prog 0 6 0x100000 ??
Can anyone help me on this.
I don't know what imx6 board you use, for fuse, you can refer to the link as below: