There seems to be a paucity of app notes on how to support Digital(PDM) microphones in the i.MX5 and i.MX6.
Has anyone used PDM mics on the i.MX5 or i.MX6 ?
The Extended audio block seems to suggest PDM can be accomplished but before I sweat out teh details, though a quick check
on the forum would help.
GSMD
We have not got your response yet and will close the diacussion. If you still need help, please feel free to
reply with an update to this discussion.
Thanks,
Yixing
GSMD
It seems your question had been answered. We are going to close the discussionin 3 days if you are fine .
Thanks,
Yixing
Hi gsmd,
As Brad mentioned, none of our imx family audio interfaces (SSI, ESAI, SAI) are equpped with PDM receiving capability.
Our recommendations are following.
1. Use Codec such as WM8962 to interface PDM digital microphone then have the I2S output of the codec connected to one of i.MX's audio interfaces.
2. Use digital microphones with I2S output and connect to one of our I2S capable ports.
Thanks.
Haku
Download the Sabre SD schematics. They have two Analog Devices ADMP5421B digital microphones connected to a Wolfson WM8962 Codec.