Custom Location provider on AOSP kitkat 4.4.2 running on IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom Location provider on AOSP kitkat 4.4.2 running on IMX6

565 Views
kulbhushankashy
Contributor I

Hi All,

I am using IMX6's based custom board and It's running android AOSP version Kitkat 4.4.2. We have cellular module and wifi connectivity but don't have GPS on board. Now We want to develop one custom location provider which will use wifi and/or cellular module to get location. How I can develop it or is there any open source application available which can do this?

Regards,

-Kulbhushan

Labels (5)
0 Kudos
1 Reply

385 Views
igorpadykov
NXP Employee
NXP Employee

Hi kulbhushan

one can try to follow suggestions given on

http://stackoverflow.com/questions/18826718/how-to-get-location-with-wifi-in-android

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos