Correct way to re-start eDMA scatter gather

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Correct way to re-start eDMA scatter gather

791件の閲覧回数
ryanshuttlewort
Contributor IV

Hello, I am using IAR with an RT1050 SDK, version  2.3.0 (2017-11-16).  I have set up a double buffered LPSPI example based on the SDK scatter gather example, however, the transaction terminates on the filling of the second buffer (last TCD) rather than restarting the whole process and buffering continuously.  So far I am only able to restart the process by going through the TCD setup again from the beginning which is very inefficient.  The linking does appear to be setup up correctly i.e. the DLAST_SGA of the last TCD links back to the first etc.

What is the correct way to make a scatter gather request run continuously?  Preferably without any software intervention once started.

No RTFM responses please.

Thanks.

0 件の賞賛
返信
1 返信

587件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  can we continue consideration under https://community.nxp.com/message/982345 ?

Regards,

Yuri.

0 件の賞賛
返信