Core Voltages Clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Core Voltages Clarification

609 Views
sudarkb
Contributor II

Why does the Core voltage ( SOC and ARM voltage domain) are being changed in most revision of IMX6 application document. The latest revision of the document specifies the values as below for LDO enabled mode.

static struct cpu_op mx6dl_cpu_op_1G[] = {
{
.pll_rate = 996000000,
.cpu_rate = 996000000,
.cpu_podf = 0,
.pu_voltage = 1275000,
.soc_voltage = 1275000,
.cpu_voltage = 1350000,},
{
.pll_rate = 792000000,
.cpu_rate = 792000000,
.cpu_podf = 0,
.pu_voltage = 1275000,
.soc_voltage = 1275000,
.cpu_voltage = 1275000,},
{
.pll_rate = 396000000,
.cpu_rate = 396000000,
.cpu_podf = 0,
.pu_voltage = 1275000,
.soc_voltage = 1275000,
.cpu_voltage = 1250000,},
};

Is this settings safe to apply to older versions of IMX6 Solo processor like processors manufactured in 2016.

Labels (2)
0 Kudos
1 Reply

553 Views
art
NXP Employee
NXP Employee

Yes, it's safe to apply the new values to earlier batches of the processors.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos