Coin cell charge current in PF3000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coin cell charge current in PF3000

ソリューションへジャンプ
841件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Considering that the coin type battery will be charged, we would like to calculate the battery life.

Please give me the maximum value of the current flowing from the PMIC to the coin type battery while the voltage is being supplied to VIN.

According to the table 29 of PF3000.pdf, typical value of coin cell charge current is 60uA and  accuracy is ±30%.

So I think the value of max and min is as follow.

Max: 78uA

Typ: 60uA

Min: 42uA

Are the above coin cell charge current values correct ?

 

Ko-hey

ラベル(3)
0 件の賞賛
返信
1 解決策
697件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the maximum charge current to fully discharged coin cell battery of the PF3000 PMIC is in range of 42uA to 78uA.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
698件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the maximum charge current to fully discharged coin cell battery of the PF3000 PMIC is in range of 42uA to 78uA.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信