Cannot talk to any of the ports of iMX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot talk to any of the ports of iMX8

635 Views
jaux_al
Contributor I

I am trying access the iMX8 over the console and when I connected the board to the host over UART cable, I saw 4 com ports.
Firstly, I'm not sure why am I seeing 4 and not just one 1.  

Secondly, I opened teraterm, set baud rate to 115200 but couldn't type anything in the serial session for any of the ports.

What could possibly be wrong?

0 Kudos
2 Replies

624 Views
b36401
NXP Employee
NXP Employee

Are you sure the processor boots some valid image?
Please note that the bootROM itself does not use UART for the diagnostic console.
So first it should get something like u-boot and then you will see the console.

Please refer to this article regarding to boot process:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...

0 Kudos

614 Views
jaux_al
Contributor I

I am using the following to flash the image...

bunzip2 -dk -f core-image-minimal-imx8qxpmek.sdcard.bz2 
sudo dd if=core-image-minimal-imx8qxpmek.sdcard of=/dev/sdb bs=1M conv=fsync

 and i see the SD card has .dtf files as well as the image file. Shouldn't that be enough?

0 Kudos