Can the cores interrupt each other in i.MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the cores interrupt each other in i.MX6?

Jump to solution
1,447 Views
JimSung
Contributor I

Can the cores interrupt each other in i.MX6?  I don't see it in the reference manual.

Labels (2)
0 Kudos
1 Solution
838 Views
YixingKong
Senior Contributor IV


JimSung, did MaxTsai andswer your question? If yes, please click Correct Answer so that we can close the DI.

Thanks,

View solution in original post

0 Kudos
6 Replies
838 Views
max_tsai
NXP Employee
NXP Employee

hi, you may refer to "uboot-imx/include/asm-arm/arch-mx6/mx6.h"

/* Cortex-A9 MPCore private memory region */

#define ARM_PERIPHBASE              0x00A00000

#define SCU_BASE_ADDR               (ARM_PERIPHBASE)

#define IC_INTERFACES_BASE_ADDR     (ARM_PERIPHBASE + 0x0100)

#define GLOBAL_TIMER_BASE_ADDR      (ARM_PERIPHBASE + 0x0200)

#define PRIVATE_TIMERS_WD_BASE_ADDR (ARM_PERIPHBASE + 0x0600)

#define IC_DISTRIBUTOR_BASE_ADDR    (ARM_PERIPHBASE + 0x1000)

0 Kudos
839 Views
YixingKong
Senior Contributor IV


JimSung, did MaxTsai andswer your question? If yes, please click Correct Answer so that we can close the DI.

Thanks,

0 Kudos
838 Views
max_tsai
NXP Employee
NXP Employee

hi Jim,

I may not get your point. ARM multiple-cores use the same interrupt controller, and it seems unable to interrupt specific CPU core by this controller.

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0407e/CCHDBEBE.html

0 Kudos
838 Views
max_tsai
NXP Employee
NXP Employee

Correct my previous reply. This register can meet the requirement.

Software Generated Interrupt Register (ICDSGIR)

[23:16]CPUTargetList

When TargetList Filter = 0b00, defines the CPU interfaces the Distributor must send the interrupt to.

Each bit of CPUTargetList[7:0] refers to the corresponding CPU interface, for example CPUTargetList[0] corresponds to CPU interface 0. Setting a bit to 1 sends the interrupt to the corresponding interface.

//"arch/arm/common/gic.c"

508 #ifdef CONFIG_SMP

509 void gic_raise_softirq(const struct cpumask *mask, unsigned int irq)

510 {

511         unsigned long map = *cpus_addr(*mask);

512

513         /*

514          * Ensure that stores to Normal memory are visible to the

515          * other CPUs before issuing the IPI.

516          */

517         dsb();

518

519         /* this always happens on GIC0 */

520         writel_relaxed(map << 16 | irq, gic_data[0].dist_base + GIC_DIST_SOFTINT);

521 }

522 #endif


0 Kudos
838 Views
alexanderburaga
Contributor I

Could you tell what is the address of

ICDSGIR

register in the i.mx6q memory MAP?

0 Kudos