Can i change the widgets or pictures with SD-Card in working project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i change the widgets or pictures with SD-Card in working project?

417件の閲覧回数
SpeedyGonzales
Contributor I

Hello everyone,

I want to create a LCD project with i.MX processors. But i am not sure for this. I want to change widgets or pictures for the project with SD-Card. For example, the user want to change background picture and the date location and change the gui guider output. After this, puts its output on the SD card. (tCustom Board supports SD card interface) Can Picture and Widget change in the working project?

タグ(2)
0 件の賞賛
3 返答(返信)

404件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which processor are you using? Which version of BSP are you using?

What project are you talk about?

0 件の賞賛

397件の閲覧回数
SpeedyGonzales
Contributor I

Hello Jimmychan,

I am talking about iMX RT1050 - 1060 - 1160 - 1170. But It's not about the processor. Does the gui guider image or widget output need to be compiled in the MCUXpresso IDE to run on the processor? Or is it enough to just show it as a source?

0 件の賞賛

383件の閲覧回数
CarlosGarabito
NXP TechSupport
NXP TechSupport

 

Hi , yes GUIGuider image or widget need to be compiled in the MCUXpresso IDE to run on the processor

0 件の賞賛