Hello all,
Hardware:
OS:
Question:
Thank you all.
Best Regards,
Tiago Rodrigues
FlexCAN is verified on L4.9.88 BSP., we do not support in Android
The iMX8QXP default driver used CAN fd mode, so we used followed command to test it:
Rx: ip link set can0 up type can bitrate 1000000 dbitrate 4000000 fd on
Tx: ip link set can1 up type can bitrate 1000000 dbitrate 4000000 fd on
Rx: candump can0
Tx: cangen can1 -m
If you want to use the legacy mode iMX6/7 test command such as "ip link set can0 up type can bitrate 1000000", you need disable the fd mode in device tree by added "disable-fd-mode".
Hi,
So is not possible to have CAN bus access using Android Automotive OS?
Thanks in advance.