Build mxc_vpu_test for Android R10.3.2 -blog archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build mxc_vpu_test for Android R10.3.2 -blog archive

1,041 次查看
shaojun_wang
NXP Employee
NXP Employee

1. Clone linux-test from FSL git server

    git clone git://sw-git01-tx30.am.freescale.net/linux-test.git

 

2. Check out the version for r10.3.2

    git checkout 2396df8ba5af2ca4bd512dbfffeaaa8d5b5028bd

 

3. Copy vpu test code to myandroid folder and build

    mmm mxc_vpu_test

 

4. Run

    mxc-vpu-test -D "-i /mnt/sdcard/sendvpudecode.264 -f 2"

标记 (1)
0 项奖励
5 回复数

599 次查看
satellite12
Contributor I

Hi Shaojun,

Could you help to provide the binary file?

Thanks.

0 项奖励

599 次查看
GunjanSamaiya
Contributor I

Initialized empty Git repository in /home/xyz/Bsp/linux-test/.git/
fatal: Unable to look up sw-git01-tx30.am.freescale.net (port 9418) (Name or service not known)

Please helpHow to Checkout ?

0 项奖励

599 次查看
dorothyxsara
Contributor II

Thanks a lot!

0 项奖励

599 次查看
shaojun_wang
NXP Employee
NXP Employee

sw-git01-tx30.am.freescale.net is FSL internel link, please contact local FAE to get the source code.

0 项奖励

599 次查看
dorothyxsara
Contributor II

Dear sir,

fatal: Unable to look up sw-git01-tx30.am.freescale.net (port 9418)

Is this url correct?

0 项奖励