Build Yocto for BSP 4.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Yocto for BSP 4.0.0

Jump to solution
1,418 Views
MarcoSandrelli
Contributor III

Hi at all,

how can I build Yocto for iMX6 BSP 4.0.0? We have only one Yocto for all iMX6 platform like ubuntu?

Thanks!

Labels (2)
0 Kudos
Reply
1 Solution
1,055 Views
LeonardoSandova
Specialist I

Actually the release number is 1.4 and I am not sure about the release dates. Subscribe to the mailing list to cehck latest status.

Leo

View solution in original post

0 Kudos
Reply
3 Replies
1,055 Views
LeonardoSandova
Specialist I

I can not fully answer first question but after a BSP release using LTIB, Yocto moves quickly to be at the same level as ltib. In the near future, this won't be a problem because the building platform will only be Yocto. For the second question, the answer is yes,

Freescale Community BSP Release Notes 1.4a documentation

However, you need to specify the machine for each build, so there is no ONE image which boots every iMX.

Leo

1,055 Views
MarcoSandrelli
Contributor III

Hi Leo,

Thank you very much for your answer,

a release date for Yocto BSP 4.0.0?

:smileyhappy:

0 Kudos
Reply
1,056 Views
LeonardoSandova
Specialist I

Actually the release number is 1.4 and I am not sure about the release dates. Subscribe to the mailing list to cehck latest status.

Leo

0 Kudos
Reply