Broadr-reach support for i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Broadr-reach support for i.MX53

966 Views
psycloak
Contributor I

Dear All,

I am working on a project using i.MX53. Just today, I got a request for a support for Broadr-reach ethernet. Anybody knows if i.MX53 can support Broadr-reach? As google returns, the i.MX6 has Broadr-reach support. I am trying not to change the hardware. So I am thinking the possibility of USB to Broadr-reach converter. Anybody can recommend for the converter?

Thanks and have a nice day!

Best Regards,

Ian

Labels (2)
0 Kudos
1 Reply

540 Views
igorpadykov
NXP Employee
NXP Employee

Hi ian

i.MX53 has not RGMII, however its FEC supports MII,RMII

so any ethernet phy can be connected with these standard interfaces,

as for example LAN8720 in i.MX53 QSB

MCIMX53-START-R i.MX53 QS Board Schematics

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos