Booting Android on i.MX53 QSB from SD: not mounting /system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting Android on i.MX53 QSB from SD: not mounting /system

Jump to solution
1,375 Views
alexandremedeir
Contributor I

Hello, I'm trying to boot Android on my i.mx53 qsb but I'm having some problems, aparently the /system partition is not mounting, so the kernel boots but there's no program to run, the funny thing is that I get a tux picture on my vga monitor...

 

I'm using Adeneo's prebuilt Freescale-iMX53-QSB-Android 2.3-Version 4.3 image, I tried following the i.MX Android R10.3.2 User Guide to boot from SD with the prebuilt image, but encountered the same problems, the main difference is that on Adeneo's image, the adb is launched, but my computer doesn't finds any device with the adb and I only get the tux picture with Adeneo's image.

 

When I connect the usb cable on my computer I see this message on the serial output:

 

usb wakeup is here

otg udc vbus rising wakeup

android_usb gadget: high speed config #1: android


I'm attaching the serial output from boot, I think it might help.

Thanks

Original Attachment has been moved to: imx53-android-log-adeneo_prebuilt.txt.zip

Labels (2)
1 Solution
740 Views
daiane_angolini
NXP Employee
NXP Employee

How did you partition your sdcard?

I saw it on your log:

mmc0: new high speed SDHC card at address 1234

mmcblk0: mmc0:1234 SA04G 3.67 GiB

mmcblk0: unknown partition table

Does your sdcard have any partition table?

View solution in original post

0 Kudos
3 Replies
741 Views
daiane_angolini
NXP Employee
NXP Employee

How did you partition your sdcard?

I saw it on your log:

mmc0: new high speed SDHC card at address 1234

mmcblk0: mmc0:1234 SA04G 3.67 GiB

mmcblk0: unknown partition table

Does your sdcard have any partition table?

0 Kudos
740 Views
alexandremedeir
Contributor I

Thanks, I didn't notice that the script deleted the partition table, I fixed and now it's working

740 Views
daiane_angolini
NXP Employee
NXP Employee

Great!

0 Kudos