Are cameras included in the iMX6Q SDP Kit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are cameras included in the iMX6Q SDP Kit?

跳至解决方案
2,088 次查看
makislivadas
Contributor IV

Need to know if cameras are included in this kit.

SABRE Platform for Smart Devices Based on the i.MX 6 Series Product Summary Page

According to this document

https://community.freescale.com/servlet/JiveServlet/previewBody/93975-102-3-4139/ov5642-mx6qsdp-stre...

There are two suitable kits featured in the kit but is not clear to me if the cameras are included.

Anybody bought this kit here that can confirm the cameras are included?

标签 (2)
0 项奖励
1 解答
943 次查看
hippo
NXP TechSupport
NXP TechSupport

The Smart Device Platform (MCIMX6Q-SDP) include both MIPI OV5640 and CSI OV5642 modules. Customer doesn't need to buy additional module for MCIMX6Q-SDP.

For the MCIMX6Q-SDB, it only provides the CSI OV5642 module. If the customers want to use the MIPI camera on this board, they need to soldering the interface of the board by themselves then connect OV5642.

For the schematics, you can refer to MCIMX6Q-SDP's.

You may find this module with Part Numbers OV05640-MRFL-A00A/ OV5462-MRSL-A01A from vendor A-Kerr (http://www.a-kerr.com/en/content.php?cid=about). Other vendors might have similar components but these are the ones used on our SABRE Platforms.

在原帖中查看解决方案

0 项奖励
2 回复数
944 次查看
hippo
NXP TechSupport
NXP TechSupport

The Smart Device Platform (MCIMX6Q-SDP) include both MIPI OV5640 and CSI OV5642 modules. Customer doesn't need to buy additional module for MCIMX6Q-SDP.

For the MCIMX6Q-SDB, it only provides the CSI OV5642 module. If the customers want to use the MIPI camera on this board, they need to soldering the interface of the board by themselves then connect OV5642.

For the schematics, you can refer to MCIMX6Q-SDP's.

You may find this module with Part Numbers OV05640-MRFL-A00A/ OV5462-MRSL-A01A from vendor A-Kerr (http://www.a-kerr.com/en/content.php?cid=about). Other vendors might have similar components but these are the ones used on our SABRE Platforms.

0 项奖励
943 次查看
pieterpostma
Contributor I

I bought the SDB and there is NO camera module. I also can't find it on the a-kerr.com.

Are there alternatives? Are there other compatible camera's for the sabre SDB?

0 项奖励