Application Layer: IMX8MQ to IMX8MQ communication using PCIe cross-link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application Layer: IMX8MQ to IMX8MQ communication using PCIe cross-link

518 Views
harshitshah
Contributor III

Hi NXP Team,

We have gone through the reference of the below link:

i.MX6Q PCIe EP/RC Validation System 

  1. In our end application we want to establish full-duplex communication between two processors. (which might not be the video data). How we can build the same? 
  2. In the application how we can establish the synchronization between these two reads and write?  Is this something already implemented by NXP?
Labels (1)
0 Kudos
1 Reply

481 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harshit

1. these examples can be used for full-duplex communication, as pcie

has separate transmit and receive channels allowing for simultaneous

operation. If you have special task one can apply to Commercial Support and Engineering Services | NXP 

for developing such aplication.

2. I am afraid such synchronization is not implemented in nxp bsps, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos