Hello!
Everybody know that Google open Android 4.0 sources, does anybody try to port it on IMX53 QSB? I am using know 2.3 BSP from adeneo. I have build 4.0 and get system.img file , but I use make PRODUCT-generic-user not imx53_loco like in adeneo. I dont touch 2.6.35 kernel from 2.3. Could anybody give some advices what to change in sources to get it working? init, init.rc?
Does anyone knows what do i need to fix this error ? I'm running on Ubuntu 11.10 x86
I see...
Device Mount point Size
/dev/fd0 none 0MB
/dev/sda none 102400MB
/dev/sda1 / 101888MB
/dev/sda2 none 509MB
/dev/sda5 none 509MB
/dev/sdb none 3768MB
/dev/sr0 none 0MB
Are you 100% sure, on selecting [/dev/sdb] (y/n)? y
Checking that no-one is using this disk right now ...
OK
Warning: bad partition start (earliest 794625)
end of partition 4 has impossible value for cylinders: 1023 (should be in 0-1019)
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
Traceback (most recent call last):
File "./linaro-image-tools/linaro-android-media-create", line 138, in <module>
args.should_create_partitions, args.should_align_boot_part)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 66, in setup_android_partitions
get_android_partitions_for_media (media, board_config)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 372, in get_android_partitions_for_media
media.path, 1 + board_config.mmc_part_offset)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 432, in _get_device_file_for_partition_number
device_path = _get_udisks_device_path(dev_file)
File "/home/android/ICS/linaro-image-tools/linaro_image_tools/media_create/partitions.py", line 447, in _get_udisks_device_path
return udisks.get_dbus_method('FindDeviceByDeviceFile')(device)
File "/usr/lib/python2.7/dist-packages/dbus/proxies.py", line 68, in __call__
return self._proxy_method(*args, **keywords)
File "/usr/lib/python2.7/dist-packages/dbus/proxies.py", line 143, in __call__
**keywords)
File "/usr/lib/python2.7/dist-packages/dbus/connection.py", line 630, in call_blocking
message, timeout)
dbus.exceptions.DBusException: org.freedesktop.UDisks.Error.Failed: No such device
Hi, today I found Linaro's build ICS and flash it. I get not stable working ICS, but I see workscpaces, and launch Settings app. It works very buggy. Kernel is 3.1, Android 4.0.1, you could find compiled system on their site linaro.org
Hi. I´m looking forward to start working on ICS port for QSB, but I had not time yet =(
Do you know which is the kernel ICS needs? I don´t think it will be 2.6.35
I will follow this thread, so we can keep the discussion....